imx6 u-boot ltib nothing on minicom

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 u-boot ltib nothing on minicom

ソリューションへジャンプ
1,761件の閲覧回数
alexandredel
Contributor I

Hello everybody

I am trying to flash a u-boot on my sabrelite board, however, when i use imx loader with the u boot created by ltib, nothing appear on minicom. When i try with the u-boot.bin, it succeed but there is nothing on the minicom's prompt, and when i try with the u-boot, it says:

unknown load address

HAB security state: development mode (0x56787856)

And of course, there is nothing on the prompt.

Do you have an idea how to fix this?

Thanks

Alexandre

ラベル(1)
0 件の賞賛
返信
1 解決策
1,366件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Alexandre

actually sabrelite board uses own bootloaders and special methods for flashing them.

Please refer to excellent help resource below and post issue if this will not help

on boundary devices forum

http://eewiki.net/display/linuxonarm/i.MX6x+SABRE+Lite+SPI+Flash+Recovery

http://boundarydevices.com/community/

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,367件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Alexandre

actually sabrelite board uses own bootloaders and special methods for flashing them.

Please refer to excellent help resource below and post issue if this will not help

on boundary devices forum

http://eewiki.net/display/linuxonarm/i.MX6x+SABRE+Lite+SPI+Flash+Recovery

http://boundarydevices.com/community/

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信