Hi, i have a question about the opencl map(clEnqueueMapBuffer ) mechanism. if a opencl host program allocs a block of memory by itself (such as malloc) not clCreateBuffer,then it calls clEnqueueMapBuffer to map the memory to gpu.can gpu use the mapped memory directly (or DMA )without any data copy (or DMA transfer )to vivante opencl runtime lib or to gpu global memory. Any Tips?thanks
解決済! 解決策の投稿を見る。
I just checked and cl_mem must be used to allocate memory clEnqueueMapBuffer, there isn´t another way to do fill cpu buffers to be used in gpu, so, zero copies in this case is not possible.
regards,
Andre
I just checked and cl_mem must be used to allocate memory clEnqueueMapBuffer, there isn´t another way to do fill cpu buffers to be used in gpu, so, zero copies in this case is not possible.
regards,
Andre
Hi,
Is any updates or tips on it? How to make host<->opencl memory access faster?
data transfers take a half of computation time on imx6qp
I've tried this on imx6. Seems like the buffer is still copied. No any performance improvement was achieved.
I´m checking this information and will be back soon with the answer.
anyone can help me?thanks