imx6 mass production memory calibration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 mass production memory calibration

ソリューションへジャンプ
735件の閲覧回数
yairh
Contributor III

Hi, 

After reviewing  the information in

https://freescale.jiveon.com/docs/DOC-105652

https://freescale.jiveon.com/docs/DOC-346065 

We still would like to know how to run memory calibration for mass production purposes. 

It seems the the the UI version cannot be executed in "batch mode" generating calibration parameters after each cycle. The two other option described in https://freescale.jiveon.com/docs/DOC-105652 are used fro memory stress test and not generation of calibration parameters. 

Is there a way to generate calibration parameters in a non-interactive mode? We would like to run the calibration on a large sample of our product. 

 

Thanks,

Yair 

0 件の賞賛
返信
1 解決策
717件の閲覧回数
yairh
Contributor III

@Yuri 

Thanks for the information. Will review the application note. 

 

Yar

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
722件の閲覧回数
Yuri
NXP Employee
NXP Employee

@yairh 
Hello,

   Generally section 7.3 (Timing Calibrations Usage) of AN4467 (i.MX 6 Series DDR Calibration)
describes possible calibration policies.

https://www.nxp.com/docs/en/application-note/AN4467.pdf

  Usually it is enough to calibrate manually several boards from a batch under different
operation conditions and use average / median values for all boards.

  We do not have special calibration tool as You need.

Regards,
Yuri.

0 件の賞賛
返信
718件の閲覧回数
yairh
Contributor III

@Yuri 

Thanks for the information. Will review the application note. 

 

Yar

0 件の賞賛
返信