imx6 lvds 1366x768 display error color

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 lvds 1366x768 display error color

1,389 Views
sunyd
Contributor I

pastedImage_6.jpg

lvds display error color,backgorund color should be black,i have checked related parameter ,but not solved,and hdmi display well

lcd:24bit,RGB24

Labels (1)
0 Kudos
Reply
6 Replies

1,141 Views
igorpadykov
NXP Employee
NXP Employee

Hi sunyd

one can check simila issue

LVDS panel display corruption 

also one can try changing the DI clock polarity, bit to change
IPUx_DI0_GENERAL bit17

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,141 Views
sunyd
Contributor I

and if=RGB666/888 ldb=dul0,display this condition;

pastedImage_1.jpg

but, if change the ldb from dul0 to sin0,display black screen(display null)

on linux( kernel3.0 .035),display well,

just below

pastedImage_4.png

thanks

0 Kudos
Reply

1,141 Views
sunyd
Contributor I

hi,igorpadykov,

modified ("#define DI_GEN_POLARITY_DISP_CLK (1 << 17)") 1 to 0("0<< 17"),but the bad color show the same previous,

and what else to do?

thanks for yours

0 Kudos
Reply

1,141 Views
igorpadykov
NXP Employee
NXP Employee

suggest to use 1360 resolution, as strictly speaking 1366 resolution

doesn't work with the IPU and GPU because that resolution is not multiple of 8.

Best regards
igor

0 Kudos
Reply

1,141 Views
sunyd
Contributor I

hi,igo:

    the error color is still crazy, have you  any other suggestions? 

   i'm sorry to give you trouble,

 

   thanks

0 Kudos
Reply

1,141 Views
igorpadykov
NXP Employee
NXP Employee

formally this is no supported by hardware, so there are no formal suggestions.

You can just try experimenting by own luck.

Best regards
igor

0 Kudos
Reply