Hi
i have developed a new board using imx6dual and using single channel 2 die micron chipMT29PZZZ8D5BKFTF-18 W.95 and
using trace32 to intialize the lpddr2 using the script provided by the freescale.But i am not able to reset the lpddr2.
what are the steps through which i can assure whether i am able to communicate with lpddr2 itself . Can you provide me
the command through which i can read the device id etc from the lpddr2 so to ensure that my communication is happening
or not.
regards
swapnil
Hi swapnil
i.MX6DL lpddr2 configuration is given in
i.MX6DL LPDDR2 Support for L3.0.35_4.0.0
pay attention that MMDC_MDISC[LPDDR2_2CH] = 0
and make sure that the DDR-SEL field for
IOMUXC_SW_PAD_CTL_PAD_DRAM_RESET is set to '00'.
Communication with lpddr2 one can test using MRW,MRR
commands, check description of MMDCx_MDSCR in RM and example in
attached script MX6SL_EVK_LPDDR2_512MB_32bit_v0.9.inc.zip:
//============================================================================= | ||
// LPDDR2 Mode Register Writes |
//=============================================================================
setmem /32 0x021b001c =0x82018030 // MRW: BA=0 CS=0 MR_ADDR=1 MR_OP=see Register Configuration
this command writes (MRW) 0x82 data to Mode 1 register (MMDCx_MDSCR bits 6-4 =0x3, 0x3 - Load Mode Register Command),
for MRR change thses bits to 0x6.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
i tried reading lpddr2
setmem /32 0x021b001c =0x00008060 ;device info
setmem /32 0x021b001c =0x00508060;device id
setmem /32 0x021b001c =0x00608060;revision id1
setmem /32 0x021b001c =0x00708060;ervision id2
all result in MDMRR =0xFFFFFFFF
seems all are junk values. Can you suggest what could be the reason . I tried this after reset MRW command and with
other permutation nothing works.
regards
swapnil
Hi igor,
we have already checked all the pins using oscilloscope its working fine seems some issue in the lpddr2 setting only
can you cross verify the configuration that we are using in above reply.
regards
swapnil
Hi Igor,
here is the lpddr2 setting that i am using. pls let me know if my seetings are proper
//============================================================================= | |||
//init script for i.Mx6DL LPDDR2 | |||
//============================================================================= | |||
// Revision History | |||
// v01 | |||
//============================================================================= | |||
wait = on | |||
//============================================================================= | |||
// Disable | WDOG | ||
//============================================================================= | |||
setmem /16 | 0x020bc000 = | 0x30 | |
//============================================================================= | |||
// Enable all clocks (they are disabled by ROM code) | |||
//============================================================================= | |||
setmem /32 | 0x020c4068 = | 0xffffffff | |
setmem /32 | 0x020c406c = | 0xffffffff | |
setmem /32 | 0x020c4070 = | 0xffffffff | |
setmem /32 | 0x020c4074 = | 0xffffffff | |
setmem /32 | 0x020c4078 = | 0xffffffff | |
setmem /32 | 0x020c407c = | 0xffffffff | |
setmem /32 | 0x020c4080 = | 0xffffffff | |
setmem /32 | 0x020c4084 = | 0xffffffff | |
setmem /32 | 0x020c4018 = | 0x00060324 | //DDR clk to 400MHz |
// Switch PL301_FAST2 to DDR Dual-channel mapping | |||
//setmem /32 | 0x00B00000 = | 0x1 | |
//============================================================================= | |||
// IOMUX | |||
//============================================================================= | |||
//DDR IO TYPE: | |||
setmem /32 | 0x020e0774 = | 0x00080000 | // IOMUXC_SW_PAD_CTL_GRP_DDR_TYPE |
setmem /32 | 0x020e0754 = | 0x00000000 | // IOMUXC_SW_PAD_CTL_GRP_DDRPKE |
//CLOCK: | |||
setmem /32 | 0x020e04ac = | 0x00000030 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_SDCLK_0 |
setmem /32 | 0x020e04b0 = | 0x00000030 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_SDCLK_1 |
//ADDRESS: | |||
setmem /32 | 0x020e0464 = | 0x00000030 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_CAS |
setmem /32 | 0x020e0490 = | 0x00000030 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_RAS |
setmem /32 | 0x020e074c = | 0x00000030 | // IOMUXC_SW_PAD_CTL_GRP_ADDDS |
//Control: | |||
setmem /32 | 0x020e0494 = | 0x00000030 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_RESET |
setmem /32 | 0x020e04a0 = | 0x00000000 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_SDBA2 - DSE can be configured using Group Control Register: IOMUXC_SW_PAD_CTL_GRP_CTLDS |
setmem /32 | 0x020e04b4 = | 0x00000030 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_SDODT0 |
setmem /32 | 0x020e04b8 = | 0x00000030 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_SDODT1 |
setmem /32 | 0x020e076c = | 0x00000030 | // IOMUXC_SW_PAD_CTL_GRP_CTLDS |
//Data Strobes: | |||
setmem /32 | 0x020e0750 = | 0x00020000 | // IOMUXC_SW_PAD_CTL_GRP_DDRMODE_CTL |
setmem /32 | 0x020e04bc = | 0x00003030 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS0 |
setmem /32 | 0x020e04c0 = | 0x00003030 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS1 |
setmem /32 | 0x020e04c4 = | 0x00003030 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS2 |
setmem /32 | 0x020e04c8 = | 0x00003030 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS3 |
//setmem /32 | 0x020e04cc = | 0x00003030 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS4 |
//setmem /32 | 0x020e04d0 = | 0x00003030 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS5 |
//setmem /32 | 0x020e04d4 = | 0x00003030 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS6 |
//setmem /32 | 0x020e04d8 = | 0x00003030 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS7 |
//Data: | |||
setmem /32 | 0x020e0760 = | 0x00020000 | // IOMUXC_SW_PAD_CTL_GRP_DDRMODE |
setmem /32 | 0x020e0764 = | 0x00000030 | // IOMUXC_SW_PAD_CTL_GRP_B0DS |
setmem /32 | 0x020e0770 = | 0x00000030 | // IOMUXC_SW_PAD_CTL_GRP_B1DS |
setmem /32 | 0x020e0778 = | 0x00000030 | // IOMUXC_SW_PAD_CTL_GRP_B2DS |
setmem /32 | 0x020e077c = | 0x00000030 | // IOMUXC_SW_PAD_CTL_GRP_B3DS |
//setmem /32 | 0x020e0780 = | 0x00000030 | // IOMUXC_SW_PAD_CTL_GRP_B4DS |
//setmem /32 | 0x020e0784 = | 0x00000030 | // IOMUXC_SW_PAD_CTL_GRP_B5DS |
//setmem /32 | 0x020e078c = | 0x00000030 | // IOMUXC_SW_PAD_CTL_GRP_B6DS |
//setmem /32 | 0x020e0748 = | 0x00000030 | // IOMUXC_SW_PAD_CTL_GRP_B7DS |
setmem /32 | 0x020e0470 = | 0x00000030 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM0 |
setmem /32 | 0x020e0474 = | 0x00000030 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM1 |
setmem /32 | 0x020e0478 = | 0x00000030 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM2 |
setmem /32 | 0x020e047c = | 0x00000030 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM3 |
//setmem /32 | 0x020e0480 = | 0x00000030 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM4 |
//setmem /32 | 0x020e0484 = | 0x00000030 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM5 |
//setmem /32 | 0x020e0488 = | 0x00000030 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM6 |
//setmem /32 | 0x020e048c = | 0x00000030 | // IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM7 |
//============================================================================= | |||
// DDR Controller Registers | |||
//============================================================================= | |||
// Manufacturer: | Micron | ||
// Device Part Number: | MT42L128M32D1TK-25 | ||
// Clock Freq.: | 400MHz | ||
// MMDC channels: | MMDC0 | ||
// Density per CS in Gb: | 4 | ||
// Chip Selects used: | 2 | ||
// Number of Banks: | 8 | ||
// Row address: | 14 | ||
// Column address: | 10 | ||
// Data bus width | 32 | ||
//============================================================================= | |||
setmem /32 | 0x021b001c = | 0x00008000 | // MMDC0_MDSCR, set the Configuration request bit during MMDC set up |
//setmem /32 | 0x021b401c = | 0x00008000 | // MMDC1_MDSCR, set the Configuration request bit during MMDC set up |
setmem /32 | 0x021b085c = | 0x1B4700C7 | //MMDC0_MPZQLP2CTL,LPDDR2 ZQ params |
//setmem /32 | 0x021b485c = | 0x1B4700C7 | //MMDC1_MPZQLP2CTL,LPDDR2 ZQ params |
//============================================================================= | |||
// Calibration setup. | |||
//============================================================================= | |||
setmem /32 | 0x021b0800 = | 0xA1390003 | // DDR_PHY_P0_MPZQHWCTRL, enable both one-time & periodic HW ZQ calibration. |
//ca bus abs delay | |||
setmem /32 | 0x021b0890 = | 0x00400000 | // values of 20,40,50,60,7f tried. no difference seen |
//setmem /32 | 0x021b4890 = | 0x00400000 | // values of 20,40,50,60,7f tried. no difference seen |
//Read calibration | |||
setmem /32 | 0x021b0848 = | 0x40404040 | // MPRDDLCTL PHY0 |
//setmem /32 | 0x021b4848 = | 0x40404040 | // MPRDDLCTL PHY1 |
//Write calibration | |||
setmem /32 | 0x021b0850 = | 0x40404040 | // MPWRDLCTL PHY0 |
//setmem /32 | 0x021b4850 = | 0x40404040 | // MPWRDLCTL PHY1 |
//dqs gating dis | |||
setmem /32 | 0x021b083c = | 0x20000000 | |
setmem /32 | 0x021b0840 = | 0x00000000 | |
//setmem /32 | 0x021b483c = | 0x20000000 | |
//setmem /32 | 0x021b4840 = | 0x00000000 | |
//read data bit delay: (3 is the reccommended default value, although out of reset value is 0) | |||
setmem /32 | 0x021b081c = | 0x33333333 | // DDR_PHY_P0_MPREDQBY0DL3 |
setmem /32 | 0x021b0820 = | 0x33333333 | // DDR_PHY_P0_MPREDQBY1DL3 |
setmem /32 | 0x021b0824 = | 0x33333333 | // DDR_PHY_P0_MPREDQBY2DL3 |
setmem /32 | 0x021b0828 = | 0x33333333 | // DDR_PHY_P0_MPREDQBY3DL3 |
//setmem /32 | 0x021b481c = | 0x33333333 | // DDR_PHY_P1_MPREDQBY0DL3 |
//setmem /32 | 0x021b4820 = | 0x33333333 | // DDR_PHY_P1_MPREDQBY1DL3 |
//setmem /32 | 0x021b4824 = | 0x33333333 | // DDR_PHY_P1_MPREDQBY2DL3 |
//setmem /32 | 0x021b4828 = | 0x33333333 | // DDR_PHY_P1_MPREDQBY3DL3 |
//write data bit delay: (3 is the reccommended default value, although out of reset value is 0) | |||
setmem /32 | 0x021b082c = | 0xF3333333 | // DDR_PHY_P0_MPREDQBY0DL3 |
setmem /32 | 0x021b0830 = | 0xF3333333 | // DDR_PHY_P0_MPREDQBY1DL3 |
setmem /32 | 0x021b0834 = | 0xF3333333 | // DDR_PHY_P0_MPREDQBY2DL3 |
setmem /32 | 0x021b0838 = | 0xF3333333 | // DDR_PHY_P0_MPREDQBY3DL3 |
//setmem /32 | 0x021b482c = | 0xF3333333 | // DDR_PHY_P1_MPREDQBY0DL3 |
//setmem /32 | 0x021b4830 = | 0xF3333333 | // DDR_PHY_P1_MPREDQBY1DL3 |
//setmem /32 | 0x021b4834 = | 0xF3333333 | // DDR_PHY_P1_MPREDQBY2DL3 |
//setmem /32 | 0x021b4838 = | 0xF3333333 | // DDR_PHY_P1_MPREDQBY3DL3 |
//For i.mx6qd parts of versions A & B (v1.0, v1.1), uncomment the following lines. For version C (v1.2), keep commented | |||
//setmem /32 | 0x021b08c0 = | 0x24911492 | // fine tune SDCLK duty cyc to low - seen to improve measured duty cycle of i.mx6 |
//setmem /32 | 0x021b48c0 = | 0x24911492 | |
// Complete calibration by forced measurement: | |||
setmem /32 | 0x021b08b8 = | 0x00000800 | // DDR_PHY_P0_MPMUR0, frc_msr |
//setmem /32 | 0x021b48b8 = | 0x00000800 | // DDR_PHY_P0_MPMUR0, frc_msr |
//============================================================================= | |||
// Calibration setup end | |||
//============================================================================= | |||
// Channel0 - startng address 0x80000000 | |||
setmem /32 | 0x021b0004 = | 0x00020036 | // MMDC0_MDPDC |
setmem /32 | 0x021b0008 = | 0x00000000 | // MMDC0_MDOTC |
setmem /32 | 0x021b000c = | 0x33374133 | // MMDC0_MDCFG0 |
setmem /32 | 0x021b0010 = | 0x00100A82 | // MMDC0_MDCFG1 |
setmem /32 | 0x021b0014 = | 0x00000093 | // MMDC0_MDCFG2 |
//MDMISC: RALAT kept to the high level of 5. | |||
//MDMISC: consider reducing RALAT if your 528MHz board design allow that. Lower RALAT benefits: | |||
//a. better operation at low frequency, for LPDDR2 freq < 100MHz, change RALAT to 3 | |||
//b. Small performence improvment | |||
setmem /32 | 0x021b0018 = | 0x00001748 | // MMDC0_MDMISC |
setmem /32 | 0x021b001c = | 0x00008000 | // MMDC0_MDSCR, set the Configuration request bit during MMDC set up |
setmem /32 | 0x021b002c = | 0x0F9F26D2 | // MMDC0_MDRWD |
setmem /32 | 0x021b0030 = | 0x00000010 | // MMDC0_MDOR |
setmem /32 | 0x021b0038 = | 0x00190778 | // MMDC0_MDCFG3LP |
setmem /32 | 0x021b0040 = | 0x00000017 | // Chan0 CS0_END |
setmem /32 | 0x021b0400 = | 0x11420000 | // MMDC0_MAARCR ADOPT optimized priorities. Dyn jump disabled |
setmem /32 | 0x021b0000 = | 0xC3110000 | // MMDC0_MDCTL |
// Channel1 - starting address 0x10000000 | |||
//setmem /32 | 0x021b4004 = | 0x00020036 | // MMDC1_MDPDC |
//setmem /32 | 0x021b4008 = | 0x00000000 | // MMDC1_MDOTC |
//setmem /32 | 0x021b400c = | 0x33374133 | // MMDC1_MDCFG0 |
//setmem /32 | 0x021b4010 = | 0x00100A82 | // MMDC1_MDCFG1 |
//setmem /32 | 0x021b4014 = | 0x00000093 | // MMDC1_MDCFG2 |
//MDMISC: RALAT kept to the high level of 5. | |||
//MDMISC: consider reducing RALAT if your 528MHz board design allow that. Lower RALAT benefits: | |||
//a. better operation at low frequency, for LPDDR2 freq < 100MHz, change RALAT to 3 | |||
//b. Small performence improvment | |||
//setmem /32 | 0x021b4018 = | 0x00001748 | // MMDC1_MDMISC |
//setmem /32 | 0x021b401c = | 0x00008000 | // MMDC1_MDSCR, set the Configuration request bit during MMDC set up |
//setmem /32 | 0x021b402c = | 0x0F9F26D2 | // MMDC1_MDRWD |
//setmem /32 | 0x021b4030 = | 0x00000010 | // MMDC1_MDOR |
//setmem /32 | 0x021b4038 = | 0x00190778 | // MMDC1_MDCFG3LP |
//setmem /32 | 0x021b4040 = | 0x00000017 | // Chan1 CS0_END |
//setmem /32 | 0x021b4400 = | 0x11420000 | // MMDC1_MAARCR ADOPT optimized priorities. Dyn jump disabled |
//setmem /32 | 0x021b4000 = | 0xC3110000 | // MMDC1_MDCTL |
// Channel0 : Configure DDR device: | |||
//CS0 | |||
setmem /32 | 0x021b001c = | 0x003F8030 | // MRW: BA=0 CS=0 MR_ADDR=63 MR_OP=0 |
setmem /32 | 0x021b001c = | 0xFF0A8030 | // MRW: BA=0 CS=0 MR_ADDR=10 MR_OP=ff |
setmem /32 | 0x021b001c = | 0x82018030 | // MRW: BA=0 CS=0 MR_ADDR=1 MR_OP=c2 |
setmem /32 | 0x021b001c = | 0x04028030 | // MRW: BA=0 CS=0 MR_ADDR=2 MR_OP=6. tcl=8, tcwl=4 |
setmem /32 | 0x021b001c = | 0x02038030 | // MRW: BA=0 CS=0 MR_ADDR=3 MR_OP=2.drive=240/6 |
//CS1 | |||
setmem /32 | 0x021b001c = | 0x003F8038 | // MRW: BA=0 CS=1 MR_ADDR=63 MR_OP=0 |
setmem /32 | 0x021b001c = | 0xFF0A8038 | // MRW: BA=0 CS=1 MR_ADDR=10 MR_OP=ff |
setmem /32 | 0x021b001c = | 0x82018038 | // MRW: BA=0 CS=1 MR_ADDR=1 MR_OP=c2 |
setmem /32 | 0x021b001c = | 0x04028038 | // MRW: BA=0 CS=1 MR_ADDR=2 MR_OP=6. tcl=8, tcwl=4 |
setmem /32 | 0x021b001c = | 0x02038038 | // MRW: BA=0 CS=1 MR_ADDR=3 MR_OP=2.drive=240/6 |
// Channel1 : Configure DDR device: | |||
//CS0 | |||
//setmem /32 | 0x021b401c = | 0x003F8030 | // MRW: BA=0 CS=0 MR_ADDR=63 MR_OP=0 |
//setmem /32 | 0x021b401c = | 0xFF0A8030 | // MRW: BA=0 CS=0 MR_ADDR=10 MR_OP=ff |
//setmem /32 | 0x021b401c = | 0x82018030 | // MRW: BA=0 CS=0 MR_ADDR=1 MR_OP=c2 |
//setmem /32 | 0x021b401c = | 0x04028030 | // MRW: BA=0 CS=0 MR_ADDR=2 MR_OP=6. tcl=8, tcwl=4 |
//setmem /32 | 0x021b401c = | 0x02038030 | // MRW: BA=0 CS=0 MR_ADDR=3 MR_OP=2.drive=240/6 |
//CS1 | |||
//setmem /32 | 0x021b401c = | 0x003F8038 | // MRW: BA=0 CS=1 MR_ADDR=63 MR_OP=0 |
//setmem /32 | 0x021b401c = | 0xFF0A8038 | // MRW: BA=0 CS=1 MR_ADDR=10 MR_OP=ff |
//setmem /32 | 0x021b401c = | 0x82018038 | // MRW: BA=0 CS=1 MR_ADDR=1 MR_OP=c2 |
//setmem /32 | 0x021b401c = | 0x04028038 | // MRW: BA=0 CS=1 MR_ADDR=2 MR_OP=6. tcl=8, tcwl=4 |
//setmem /32 | 0x021b401c = | 0x02038038 | // MRW: BA=0 CS=1 MR_ADDR=3 MR_OP=2.drive=240/6 |
setmem /32 | 0x021b0800 = | 0xA1390003 | // DDR_PHY_P0_MPZQHWCTRL, enable both one-time & periodic HW ZQ calibration. |
setmem /32 | 0x021b0020 = | 0x00001800 | // MMDC0_MDREF |
//setmem /32 | 0x021b4020 = | 0x00001800 | // MMDC1_MDREF |
setmem /32 | 0x021b0818 = | 0x00000000 | // DDR_PHY_P0_MPODTCTRL |
//setmem /32 | 0x021b4818 = | 0x00000000 | // DDR_PHY_P1_MPODTCTRL |
setmem /32 | 0x021b0004 = | 0x00025576 | // MMDC0_MDPDC now SDCTL power down enabled |
//setmem /32 | 0x021b4004 = | 0x00025576 | // MMDC0_MDPDC now SDCTL power down enabled |
setmem /32 | 0x021b0404 = | 0x00011006 | // MMDC0_MAPSR ADOPT power down enabled, MMDC will enter automatically to self-refresh while the number of idle cycle reached. |
//setmem /32 | 0x021b4404 = | 0x00011006 | // MMDC0_MAPSR ADOPT power down enabled, MMDC will enter automatically to self-refresh while the number of idle cycle reached. |
setmem /32 | 0x021b001c = | 0x00000000 | // MMDC0_MDSCR, clear this register (especially the configuration bit as initialization is complete) |
//setmem /32 | 0x021b401c = | 0x00000000 | // MMDC0_MDSCR, clear this register (especially the configuration bit as initialization is complete) |