Micron NAND device connected to GPMI nand controller is not detected.
Pin mux settings seems correct.
root@imx6solosabreauto:~# dmesg | grep nand
[ 0.440095] gpmi-nand 112000.gpmi-nand: Acq res
[ 0.440759] gpmi-nand 112000.gpmi-nand: gpmi Nand Init
[ 0.440805] gpmi-nand 112000.gpmi-nand: chip nr = 0
[ 0.440818] gpmi-nand 112000.gpmi-nand: CMD CTRL
[ 0.440829] gpmi-nand 112000.gpmi-nand: CMD CTRL
[ 0.440871] gpmi-nand 112000.gpmi-nand: CMD CTRL
[ 0.440883] gpmi-nand 112000.gpmi-nand: CMD CTRL
[ 0.440892] gpmi-nand 112000.gpmi-nand: CMD CTRL
[ 0.440933] gpmi-nand 112000.gpmi-nand: len is 1
[ 1.432864] gpmi-nand 112000.gpmi-nand: DMA timeout, last DMA :1
[ 1.438888] gpmi-nand 112000.gpmi-nand: Show GPMI registers :
[ 1.444667] gpmi-nand 112000.gpmi-nand: offset 0x000 : 0x21800001
[ 1.450773] gpmi-nand 112000.gpmi-nand: offset 0x010 : 0x00000000
[ 1.456891] gpmi-nand 112000.gpmi-nand: offset 0x020 : 0x00000000
[ 1.463009] gpmi-nand 112000.gpmi-nand: offset 0x030 : 0x00000000
[ 1.469111] gpmi-nand 112000.gpmi-nand: offset 0x040 : 0x00000000
[ 1.475228] gpmi-nand 112000.gpmi-nand: offset 0x050 : 0x00000000
[ 1.481330] gpmi-nand 112000.gpmi-nand: offset 0x060 : 0x0104000c
[ 1.487447] gpmi-nand 112000.gpmi-nand: offset 0x070 : 0x00010203
[ 1.493564] gpmi-nand 112000.gpmi-nand: offset 0x080 : 0x05000000
[ 1.499666] gpmi-nand 112000.gpmi-nand: offset 0x090 : 0x03023336
[ 1.505782] gpmi-nand 112000.gpmi-nand: offset 0x0a0 : 0x00000090
[ 1.511884] gpmi-nand 112000.gpmi-nand: offset 0x0b0 : 0xff000005
[ 1.518002] gpmi-nand 112000.gpmi-nand: offset 0x0c0 : 0x00000000
[ 1.524119] gpmi-nand 112000.gpmi-nand: offset 0x0d0 : 0x05010000
[ 1.530221] gpmi-nand 112000.gpmi-nand: Show BCH registers :
[ 1.535903] gpmi-nand 112000.gpmi-nand: offset 0x000 : 0x00000000
[ 1.542005] gpmi-nand 112000.gpmi-nand: offset 0x010 : 0x00000010
[ 1.548121] gpmi-nand 112000.gpmi-nand: offset 0x020 : 0x00000000
[ 1.554238] gpmi-nand 112000.gpmi-nand: offset 0x030 : 0x00000000
[ 1.560339] gpmi-nand 112000.gpmi-nand: offset 0x040 : 0x00000000
[ 1.566458] gpmi-nand 112000.gpmi-nand: offset 0x050 : 0x00000000
[ 1.572559] gpmi-nand 112000.gpmi-nand: offset 0x060 : 0x00000000
[ 1.578679] gpmi-nand 112000.gpmi-nand: offset 0x070 : 0xe4e4e4e4
[ 1.584797] gpmi-nand 112000.gpmi-nand: offset 0x080 : 0x070a4080
[ 1.590900] gpmi-nand 112000.gpmi-nand: offset 0x090 : 0x10da4080
[ 1.597016] gpmi-nand 112000.gpmi-nand: offset 0x0a0 : 0x070a4080
[ 1.603133] gpmi-nand 112000.gpmi-nand: offset 0x0b0 : 0x10da4080
[ 1.609235] gpmi-nand 112000.gpmi-nand: offset 0x0c0 : 0x070a4080
[ 1.615350] gpmi-nand 112000.gpmi-nand: offset 0x0d0 : 0x10da4080
[ 1.621453] gpmi-nand 112000.gpmi-nand: offset 0x0e0 : 0x070a4080
[ 1.627568] gpmi-nand 112000.gpmi-nand: offset 0x0f0 : 0x10da4080
[ 1.633687] gpmi-nand 112000.gpmi-nand: offset 0x100 : 0x00000000
[ 1.639790] gpmi-nand 112000.gpmi-nand: offset 0x110 : 0x00000000
[ 1.645905] gpmi-nand 112000.gpmi-nand: offset 0x120 : 0x00000000
[ 1.652007] gpmi-nand 112000.gpmi-nand: offset 0x130 : 0x00000000
[ 1.658123] gpmi-nand 112000.gpmi-nand: offset 0x140 : 0x00000000
[ 1.664239] gpmi-nand 112000.gpmi-nand: offset 0x150 : 0x20484342
[ 1.670342] gpmi-nand 112000.gpmi-nand: offset 0x160 : 0x01000000
[ 1.676457] gpmi-nand 112000.gpmi-nand: offset 0x170 : 0x00000000
[ 1.682570] gpmi-nand 112000.gpmi-nand: BCH Geometry :
[ 1.729256] gpmi-nand 112000.gpmi-nand: len is 1
[ 1.729270] gpmi-nand 112000.gpmi-nand: CMD CTRL
[ 1.729281] gpmi-nand 112000.gpmi-nand: CMD CTRL
[ 1.729290] gpmi-nand 112000.gpmi-nand: CMD CTRL
[ 1.729300] gpmi-nand 112000.gpmi-nand: I am in error
[ 1.729310] gpmi-nand 112000.gpmi-nand: Chip: 0, Error -22
[ 1.734822] gpmi-nand 112000.gpmi-nand: Chip fails
[ 1.739625] gpmi-nand 112000.gpmi-nand: len is 1
[ 1.739637] gpmi-nand 112000.gpmi-nand: len is 1
[ 1.739647] gpmi-nand 112000.gpmi-nand: len is 1
[ 1.739657] gpmi-nand 112000.gpmi-nand: len is 1
[ 1.739666] gpmi-nand 112000.gpmi-nand: len is 1
[ 1.739675] gpmi-nand 112000.gpmi-nand: len is 1
[ 1.739685] gpmi-nand 112000.gpmi-nand: len is 1
[ 1.739696] gpmi-nand 112000.gpmi-nand: len is 1
[ 1.739714] gpmi-nand 112000.gpmi-nand: CMD CTRL
[ 1.739723] gpmi-nand 112000.gpmi-nand: CMD CTRL
[ 1.739732] gpmi-nand 112000.gpmi-nand: CMD CTRL
[ 1.739742] gpmi-nand 112000.gpmi-nand: I am in error
[ 1.739752] gpmi-nand 112000.gpmi-nand: Chip: 0, Error -22
[ 1.745263] gpmi-nand 112000.gpmi-nand: Chip fails
[ 1.750065] gpmi-nand 112000.gpmi-nand: len is 1
[ 1.750074] nand: No NAND device found
[ 1.750094] gpmi-nand 112000.gpmi-nand: chip nr = -1
[ 1.750135] gpmi-nand 112000.gpmi-nand: driver registration failed: -19
Any clues to debug.
Hi kiruthika
from log seems it even can not read NAND ID,
had you checked hardware with SDK (simple NAND ID read procedure) ?
i.MX 6Series Platform SDK : Bare-metal SDK for the i.MX 6
Best regards
igor
Hi igorpadykov,
Will check and come back.
Thanks,
Kirthika
Hi Kirthika,
Did you have to change anything in the device tree or driver to get the NAND to work?
Thanks,
Akshay
Hi Akshay,
I added the following lines to DTS file
1. &gpmi {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_gpmi_nand_1>;
status = "okay";
};
2. Make sure that pins of pinctrl_gpmi_nand_1 is not muxed with any other devices.
With kernel configs enabled for GPMI NAND it works straight away.
Thanks,
Kirthika
Thanks for the quick reply, setting the correct pinmux fixed my issue. Appreciate your help :smileyhappy: