imx6 WebGL performance?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 WebGL performance?

822 Views
woutervh
Contributor IV

Can somebody explain me what to expect from webgl on a imx6qd board? I have compiled qtwebengine and am running a qt-application in eglfs. When I run a webgl site, it works, but not smooth. Not everything gets rendered too.

However, the CPU load of the qtwebengine process looks rather low (10%-20%) so I have the impression it's not running in software mode. But the performance is that bad, that I cannot imagine that this is the best it can do...

Anybody knows what to expect? Or how I can tweak?

Thanks

Tags (2)
0 Kudos
1 Reply

489 Views
mayqueen
Contributor IV

I have same issue, my customers complain for their HTML5 game is very no smooth, we use Chrome on Android 7.1 using imx6Q platform, CPU looks only spend 50% usage, vmalloc=512M, it's not make sense running without smooth, how to improve?

Resolution: 720P

0 Kudos