Hello,
we are using Android M6.0.1_2.1.0 to a custom hardware with i.mx6dl.
It is possible to configure eth0 with a static ip address using the Freescale Ethernet App. But after a factory reset this configuration is deleted. We need to add a static ip configuration to system.img.
Is it possible to do a static ip configuration on default (in system.img)? What it the best way to do it?
Regards,
Ludwig
if you used wifi, pls refer to the link as below:
How do I set a static IP address in the Android Operating System?
if you use ethernet port, you can use "ifconfig" to set static ip address, like
"ifconfig eth0 <IP ADDRESS>"
Thank you for the infomation.
I am still not sure how to do it. When I set a static IP with "ifconfig eth0 .... " it works. But when I start the Freescale Ethernet App an run "Check" than it does configure DHCP again.
Any idea?