imx53qsb amd-gpu(amd z430) minimum memory requirement.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx53qsb amd-gpu(amd z430) minimum memory requirement.

1,435 次查看
rayssadet
Contributor I

Hi:

Does anyone know the minimum memory requirement
for the amd-gpu in imx53qsb. ???
sure the board has enough memory but i am try to use
a scaled down version but so far up to 512MB i am getting
error from heavy graphics application.

Is there some documents stating this ??

thanks

:RAYS

标签 (2)
0 项奖励
回复
2 回复数

1,160 次查看
maxmustermann
Contributor I

BIG FAT WARNING:

Do NOT use the proprietary kernel / kgsl stuff. It's full of horrible security bugs and broken by design.

It gives the userland *FULL PHYSICAL* bus access - there's *NO SECURITY* anymore !

[imx53] WARNING! Do NOT use the proprietary GPU drivers / KGSL stuff - MAJOR RISK!

0 项奖励
回复

1,160 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Rays

as states i.MX53_START_Linux_BSP_Release_Note.pdf

gpu_memory =128M - memory reserved for the GPU.

IMX53_1109_LINUXDOCS_BUNDLE

also check attached document with memory usage.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------