I'm stepping through the steps and here are a few issues that I have found: Please note I'm working with Ubuntu:
7.3.5 - Configure tftp server
I do not have "/etc/inetd.conf" or "/etc.default/atftpd". I also do not have "/etc/exports" is this a new file?
Do I need this to compile code for the imx53?
I skipped this and continued on and then ran into:
"user@ubuntu:~/imx53/11.09.01/L2.6.35_11.09.01_ER_source$ ls
EULA install ltib.tar.gz package_manifest.txt pkgs redboot_201003.zip tftp.zip"
"~/imx53/11.09.01/L2.6.35_11.09.01_ER_source$" directory of file does not exist, if I take the $ off it says this is a directory. What is this looking for? This is a directory but I'm not sure what it is looking for.
已解决! 转到解答。
Please use the next topic how to prepare virtual machine for LTIB.
https://community.freescale.com/message/294343#294343
Please pay attention on files "Create-Ubuntu11-10-ltib11-09-01.docx" and "ubuntu-ltib-patch.tgz", linked there.
I tried the described approach on Ubuntu 12.04 - it works.
Hi Yuri
Haven't heard from you in a while. Any luck on getting some information together for me? I have the serial port opening and writing however I can't seem to get it o read. It returns a -1 which I believe is an error. I would like to start trying to connect to a database.
Please let me know
Leonard.
Sent from my iPhone
I found it. I didn't extract "linux-imx5-g++.tar.gz" This is where
that directory is. I've attached my Make file (MakeSample). I'd
appreciate it if you could take a look at it. I also attached a c file
that Ia programmer was working on before I took over.
I need an easy environment that I can do the following on the imx53:
1) open a com port
2) open a ethernet port and connect to a mysql database
3) display a series of pictures or videos
4) once screen is touched, display a numeric keypad for user to enter a
number.
5) once user has entered a uvalid number the display will display name
and a point value along with the pictures and video.
Would GNome work or QT. Are these the same type tools? I looked for
GNOME and didn't have much luck, can you attach the pdf?
Thanks
Leonard
As for
"... an easy environment that I can do the following on the imx53:
1) open a com port
2) open a ethernet port and connect to a mysql database
..."
Sounds good, but I am afraid this will require some time even to find proper docs
and instructions how to implement such project.
Would you like some part time work?
I agree, the more I dig into this the more I'm seeing it's not going to
be easy. Lets start with the com port and the QT install?
What would your approach be?
Thanks
Leonard
Tried this and there was a confilct. Something has to give. I've been
here for hours and 0 lines of code.
1. Install Eclipse.
sudo apt-get install eclipse
2. Then start Eclipse.
3. Help -> Install new software.
4. Click: Add
Name : CDT
Location : http://download.eclipse.org/tools/cdt/releases/galileo
5. In CDT Main feature, check:
Eclipse C/C++ development tools. (Binary runtime and user
documentation.)
6. In CDT optional feature:
CDT GNU Toolchain Build Support.
CDT GNU Toolchain Debug Support.
CDT Utilities.
Eclipse C/C++ Development Platform.
7. Restart Eclipse.
8. Perfect !!!
I still cannot open a c project. I'm so frustrated now. I added what you suggested. What else do I have to do? I want to be able to move on and install QT. I should of had some of this completed by now.
Sent from my iPhone
I would agree, but I take out printf and it compiles, I add a int x; and
it compiles. I'm trying to add the plug ins for eclipse and it looked
as it it worked but I still do not have a c project. If anything it
removed Java and now I have general and cvs to choose from under New
Project. I must be getting tired or I'm missing something. I was going
to try and install eclipse from scratch and I downloaded a zip file that
I was supposed to extract into a directory and I can't run that.
Frustrated!
The distro package from the Web is "L2.6.35_11.09.01_ER_source.tar.gz".
It should be unpacked in order to get the following structure of files and directories :
EULA
install
ltib.tar.gz
package_manifest.txt
pkgs
redboot_201003.zip
tftp.zip
Next - just run ./install
Yuri
I have this I'm currently at the install tlib. the command is "./tlib"
I'm getting
"I ran the command: sudo -S -l which returned :
sudo passwd for leonard: Sorry, try again
This means you do not have permission to execute rpm commands asa root."
can you tell me how to get around this?
thanks
Leonard