imx53 i2c1 on (PAD_EIM_D21 and PAD_EIM_D28)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx53 i2c1 on (PAD_EIM_D21 and PAD_EIM_D28)

Jump to solution
1,618 Views
cyrilcrocquesel
Contributor II

Hi,

I would like on a mx53 QSB the i2c1 on pin :

IMX53_PAD_EIM_D21_I2C1_SCL,

IMX53_PAD_EIM_D28_I2C1_SDA,

I've added this two line in mx53_loco_pads[] in arch/arm/mach-mx5/board-mx53_loco.h (in linux 2.6.38 from freescale). And remove this line :

MX53_PAD_EIM_D21__IPU_DISPB0_SER_CLK,

When the linux boot /dev/i2c-0 is created but I've no signal on scl or sda pin.

What is missing in my modification?

Cordially,

Cyril crocquesel

Labels (1)
0 Kudos
Reply
1 Solution
990 Views
jimmychan
NXP TechSupport
NXP TechSupport

For your reference, attached is the BSP porting guide. There is talk about porting I2C. Although it is for i.MX6, the porting is similar to i.MX53.

View solution in original post

0 Kudos
Reply
1 Reply
991 Views
jimmychan
NXP TechSupport
NXP TechSupport

For your reference, attached is the BSP porting guide. There is talk about porting I2C. Although it is for i.MX6, the porting is similar to i.MX53.

0 Kudos
Reply