Dear All,
The linux-2.6.35 is older version, so I would like to turn to linux-3.0.35, but it is not smooth.
Chosen Linux 3.0.35-imx from the menu of "./ltib -m config", then type ./ltib for building. I got the error message:
Processing: kernel-3.0.35
===========================
Build path taken because: build key set, no prebuilt rpm,
Testing network connectivity
OK GPP:
Try linux-3.0.35.tar.bz2.md5 from the GPP
http://bitshrine.org/gpp/linux-3.0.35.tar.bz2.md5:
15:37:40 ERROR 404: Not Found.
Try linux-3.0.35.tar.bz2 from the GPP
http://bitshrine.org/gpp/linux-3.0.35.tar.bz2:
15:37:40 ERROR 404: Not Found.
Can't get: linux-3.0.35.tar.bz2 at ./ltib line 802.
f_buildrpms() returned an error, exiting
traceback:
main:572
Started: Wed Dec 9 15:37:33 2015
Ended: Wed Dec 9 15:37:40 2015
Elapsed: 7 seconds
These packages failed to build:
kernel-3.0.35
Build Failed
Exiting on error or interrupt
Ok, I thought the linux-3.0.35.tar.bz2 could not be downloaded. so I downloaded from:
linux-3.0.35.tar.bz2 [73.29 MiB] - MD5: 70bda6ecf3c498b23d2ced776479a8c3 - Fileinformation
and placed to /opt/freescale/pkgs directory, create the linux-3.0.35.tar.bz2.md5 manually, then run ./ltib again, got another error:
Processing: kernel-3.0.35
===========================
Build path taken because: build key set, no prebuilt rpm,
Testing network connectivity
OK GPP:
Try linux-3.0.35-imx_10.12.01.bz2.md5 from the GPP
http://bitshrine.org/gpp/linux-3.0.35-imx_10.12.01.bz2.md5:
17:00:32 ERROR 404: Not Found.
Try linux-3.0.35-imx_10.12.01.bz2 from the GPP
http://bitshrine.org/gpp/linux-3.0.35-imx_10.12.01.bz2:
17:00:33 ERROR 404: Not Found.
Can't get: linux-3.0.35-imx_10.12.01.bz2 at ./ltib line 802.
f_buildrpms() returned an error, exiting
traceback:
main:572
Started: Wed Dec 9 17:00:29 2015
Ended: Wed Dec 9 17:00:33 2015
Elapsed: 4 seconds
These packages failed to build:
kernel-3.0.35
Build Failed
Exiting on error or interrupt
Hmmm...... now, the linux-3.0.35-imx_10.12.01.bz2 could not be download, and I could not find this file by google.
Could anyone provide some helps? Thanks in advance!
Best Regards,
Kinly,
已解决! 转到解答。
3.0.35 does not support mx28.
If you plan to update your kernel, then you could use something more recent, such as 4.3 kernel.
Also, LTIB is not supported anymore, so you could try Yocto instead.
Regards,
Fabio Estevam
3.0.35 does not support mx28.
If you plan to update your kernel, then you could use something more recent, such as 4.3 kernel.
Also, LTIB is not supported anymore, so you could try Yocto instead.
Regards,
Fabio Estevam