imx25 USB: Full speed only

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx25 USB: Full speed only

801 次查看
rohith1z
Contributor III

I want to be able to run the OTG USB port on imx25 in Full speed only mode. What's the best way to do it?

I'm using the on-board UTMI phy.

The reference manual says that:

Software-configurable for full-speed / low-speed interface for Serial transceiver

The only reference I found was bit 24(PFSC) of PORTSCx register.

Is that the recommended method?

标记 (2)
0 项奖励
回复
1 回复

723 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Look at the following https://community.nxp.com/message/262460 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复