Hi,
I can build the WIC file for the i.MX93 EVK using Yocto. I am trying now to build the flash.bin (u-boot) file for the same platform outside Yocto. Can anyone point out where to find the imx-mkimage sources that will include support for iMX9?
I am able to build successfully the u-boot.bin and related artifacts using u-boot source tree (https://github.com/u-boot/u-boot.git) with these commands:
make imx93_11x11_evk_defconfig
make
However, I am getting a Makefile errors when I try building the flash.bin:
make flash.bin
...
make[1]: *** No rule to make target 'u-boot.cnt'. Stop.
make: *** [Makefile:1520: u-boot.cnt] Error 2
Any idea how to build a single flash.bin, with no Yocto support, so it can be deployed to an eMMC or an SD.
Any input appreciated.
Thanks!
解決済! 解決策の投稿を見る。
refer to the release note
you can use this command to download
wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/<package file name>
you can find container images there
the imx-mkimage is from:
https://github.com/nxp-imx/imx-mkimage/tree/lf-6.1.22_2.0.0
pls refer to the chapter 4.5.13 How to build imx-boot image by using imx-mkimage
https://www.nxp.com.cn/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf
Under section 4.5.13, for i.MX 93 in Step 3, it says: Copy the image of Sentinel firmware container mx93a0-ahab-container.img to imx-mkimage/iMX9/
I used mx93a0-ahab-container.img from the Yocto build results and was able to successfully build and deploy flash.bin.
Is there a way to build mx93a0-ahab-container.img artifact independently, outside of Yocto?
refer to the release note
you can use this command to download
wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/<package file name>
you can find container images there