imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x40000000

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x40000000

跳至解决方案
1,330 次查看
yongheluo_hotma
Contributor III

Hi,

    When I use IPU to resize image. Sometimes, it was failed and kernel panic. (The image resolution is : 1280 x 720)

    I get the flowing error:

    " imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x40000000 "

   Thanks.

    Yonghe.Luo

0 项奖励
回复
1 解答
1,016 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yonghe.Luo

IPU_INT_STAT_10 = 0x40000000 means AXI read access error, one can check

programming requirements provided for AXIR units in sect.37.4.2.4.1 Handling real time channels,

37.4.2.5, Table 37-15 i.MX6DQ Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,017 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yonghe.Luo

IPU_INT_STAT_10 = 0x40000000 means AXI read access error, one can check

programming requirements provided for AXIR units in sect.37.4.2.4.1 Handling real time channels,

37.4.2.5, Table 37-15 i.MX6DQ Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,016 次查看
yongheluo_hotma
Contributor III

Dear Igor,

     Thanks.

    

    Yonghe.Luo

0 项奖励
回复