imx-gpu-viv-1_5.0.11.p8.7-hfp.bin is not available

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx-gpu-viv-1_5.0.11.p8.7-hfp.bin is not available

846 次查看
hartmutbehrensf
Contributor I

Hi,

The latest ARM Yocto BSP, codename imx-morty (fsl-arm-yocto-bsp.git - i.MX Linux BSP Release Yocto Project manifests ) attempts to fetch http://www.freescale.com/lgfiles/NMG/MAD/YOCTO/imx-gpu-viv-1_5.0.11.p8.7-hfp.bin during the do_fetch task of imx-gpu-viv-1_5.0.11.p8.7-hfp recipe. 

Unfortunately, a "404 Not Found" response is returned and the task fails to fetch the relevant files.

Is it possible for the Vivante driver imx-gpu-viv-1_5.0.11.p8.7-hfp.bin to be made available at the http://www.freescale.com/lgfiles/NMG/MAD/YOCTO so that the imx-morty BSP can be built please ?

0 项奖励
回复
1 回复

540 次查看
joanxie
NXP TechSupport
NXP TechSupport

the official version is p8.6, P8.7 is just for internal testing, pls try to use p8.6.

0 项奖励
回复