imx-4.19.35-1.1.0.xml updated to incorrect SHA for https://source.codeaurora.org/external/imx

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx-4.19.35-1.1.0.xml updated to incorrect SHA for https://source.codeaurora.org/external/imx

377 次查看
vincentz63
Contributor IV

File imx-4.19.35-1.1.0.xml in repo https://source.codeaurora.org/external/imx/imx-manifest was updated to pull the wrong revision for the CAF repo:

- <project remote="CAF" revision="6b237a975521daa1687c5ac49f57da6d32c8c719" name="meta-fsl-bsp-release" path="sources/meta-fsl-bsp-release" upstream="warrior-4.19.35-1.1.0" >
+ <project remote="CAF" revision="b2c6e41596b8d068232e0a5fddf2675aa57ec92a" name="meta-fsl-bsp-release" path="sources/meta-fsl-bsp-release" upstream="warrior-4.19.35-1.1.0" >

The update was done in commit 0d1e92b4b7d432fb9456fc9fcdf3586114c6fbda by Tom Hochstein <tom.hochstein@nxp.com> on Wed Apr 6 16:24:27 2022 -0500.

The next commit replaces the SHA with a tag name, and is also invalid.

I believe this is a mistake as this commits changes the source code used for an existing release, which should never happen, and breaks the build in the process! (It no longer overwrites the meta-freescale machine conf files.)

标记 (2)
0 项奖励
0 回复数