Hi,
I'm running bare metal on iMx25 PDK with debug board.
I'm trying to access UART register (USR1) on user mode but each time it raise a data abort.
Is hardware register only accessible from privileged mode ?
Documentation says I can read/write as user, may be I miss to configure a register but i don't know which one.
This is the exemple code I made to read USR1 at the boot.
start_boot:
// After a reset, the mode is ARM, Supervisor, interrupts disabled.
// Invalidate both ICache and DCache : not done upon emulator reset
ldr r1,=0
mcr p15,0,r1,c7,c7,0
// Disable MMU translation, D cache and enable I cache
mrc p15,0,r1,c1,c0,0
ldr r0,=CP_DIS_MASK // 0xFFFFEFFA
and r1,r1,r0
orr r1,r1,#(1<<12)
orr r1,r1,#2
mcr p15,0,r1,c1,c0,0
// Initialize clocks
bl | low_level_init |
// Switch to user and try access USR1
bic r0,r0,#MODE_MSK // Clear the mode bits
orr r0,r0,#USR_MODE // Set USER mode bits
msr cpsr_c,r0
ldr r3, =0x43f90098
ldr r3,[r3]
If you have any idea why I can't access uart register in user mode, any help is welcome.
Thanks in advance.
Simon
解決済! 解決策の投稿を見る。
Hi Simon
this may be related with AIPS priviledge settings,
suggest to create service request for obtaining
AIPS description.
Best regards
igor
You solve my problem. Thank's a lot igor !
Ok thank's, I have misunderstood.
Hi Simon
AIPS chapter is not present in RM, you can
obtain it creating service request
Best regards
igor
Hi Igor,
Sorry for the wait,
I didn't found much information about AIPS registers in the iMx25 doc.
The AIPS A configuration seems to be made by MAX module.
I looked at my MAX description, but it seems good, all access restriction are disabled ...
Best regards
Simon
Hi Igor
I tried with module clock enabled and disabled for my Uart but I have always the same problem.
When I'm tring to access Uart register in privileged mode, in the same terms it's working.
I thing I have a permission access problem.
I check all my config and none register seems to enable a module which manage access permisson.
So I don't know where problem come from. May be from boot.
I load my program in RAM direclty with JTAG and configure the iMx25 PDK to boot on SD Card.
Hi Simon
this may be related with AIPS priviledge settings,
suggest to create service request for obtaining
AIPS description.
Best regards
igor
Hi Simon
register may be not accessible when module clock is gated
in CCM, so one can check uart bits in CGCRx registers.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------