iMX93 USB 2.0 device tree node undefined

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX93 USB 2.0 device tree node undefined

1,430件の閲覧回数
AlanWen
Contributor IV

I'm using the iMX93 EVK board porting USB 2.0 device tree, the original source code is porting fort type-C.
I'd tried to post the code below in u-boot dts (imx93-11x11-evk.dts) but it doesn't work.

reg_usb0_host_vbus: regulator-usb0-vbus {
		compatible = "regulator-fixed";
		regulator-name = "usb0_host_vbus";
		regulator-min-microvolt = <5000000>;
		regulator-max-microvolt = <5000000>;
		enable-active-high;
		regulator-always-on;
	};

 

Also, I tried to modify the usb node for switching to host mode as below. It seems not a correct way to port USB as host.

&usbotg1 {
	dr_mode = "host";
	status = "okay";
};

 

And then modifying the configuration in imx93-11x11_evk_defconfig.

# CONFIG_USB_TCPC is not set
CONFIG_IMX_HAB=y


How can I modify the code for USB 2.0 ?
Could you please provide a complete sample code

 

Thanks

タグ(5)
0 件の賞賛
返信
1 返信

1,402件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

According to Reference Manual p. 90 you should make it with dr_mode change made. Could you try to remove the config:

 

[*] ChipIdea device controller

 

Or is this issue only persistent in u-boot?

Also, is your work over an EVK or custom board? i.MX 93 processor has USB 2.0 already,

Regards

0 件の賞賛
返信