iMX93 EVK LVDS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX93 EVK LVDS

2,345 次查看
coilnpark
Contributor IV

Hi,

I am using iMX93 11x11 evk.

When I checked LVDS Clock and signals in this evk board with the offered OS image full version from NXP, LVDS clock didn't output.

Is there any setting to output LVDS?

标记 (1)
0 项奖励
回复
3 回复数

2,317 次查看
Nobita
Contributor III

I use imx93-11x11-evk-boe-wxga-lvds-panel.dtb and the lvds panel works well, I think it's enough for you to check the clock with the same dtb file.
The imx93-11x11-evk-boe-wxga-lvds-panel dts does enable the lvds releated nodes and does disable the DSI2MIPI related nodes. I am not an expert, I am also consulting NXP's engineer about how to enable dual display with the same video output via hdmi and lvds.  

0 项奖励
回复

2,329 次查看
Nobita
Contributor III

Have you change your dtb file since the default dtb does not enable lvds releated nodes.

0 项奖励
回复

2,321 次查看
coilnpark
Contributor IV

Thank  you for your reply.

I tried to change the below file.
But it didn't work.
Do I have to change more?

arch/arm64/boot/dts/freescale/imx93-11x11-evk.dts



lvds_backlight: lvds_backlight {
              compatible = "pwm-backlight";
              pwms = <&tpm4 1 50000 0>;
              brightness-levels = <0 20 25 30 35 40 100>;
              default-brightness-level = <4>;
              status = "okay";
};

lvds_panel {
              compatible = "innolux,g121x1-l03","simple-panel";
              backlight = <&lvds_backlight>;

              port {
                          panel_lvds_in: endpoint {
                                      remote-endpoint = <&lvds_out>;
                          };
              };

};



&ldb {
              status = "okay";

              lvds-channel@0 {
                          status = "okay";

                          port@1 {
                                      reg = <1>;

                                      lvds_out: endpoint {
                                                  remote-endpoint = <&panel_lvds_in>;
                                      };
                          };
              };
};

&ldb_phy {
              status = "okay";
};

0 项奖励
回复