iMX8m Nano GPU GC7000UL slow

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX8m Nano GPU GC7000UL slow

1,690 次查看
miguel_deprado
Contributor II

Hi,

I have an iMX8m Nano flashed with Yocto image: 

repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.47-2.2.0.xmlimx-manifest - i.MX Release Manifest

DISTRO=fsl-imx-xwayland MACHINE=imx8mnevk source imx-setup-release.sh -b build_nano

I've tested a openCL benchmark on the board and I'm only getting 2 GLOPs compared to the 9.6 GLOPs in the board specifications. I've performed the same test on the quad-max board, getting 20 GLOPs compared to the 32 theoretical GLOPs. As a rule of thumb, I should get around 6 GLOPs on the iMX8m Nano based on the quad-max results.

I can see that the freq of the GPU core and shader is well set to 600 MHz, but the performance is low.

Is there any configurations that I might be missing?

Thanks

标签 (1)
0 项奖励
回复
5 回复数

909 次查看
ItamarE
Contributor I

Any news about this?

Trying to operate the IMX8-Nano GPU.

0 项奖励
回复

1,525 次查看
miguel_deprado
Contributor II

Hi,

Any update on this issue?

Best regards

0 项奖励
回复

1,680 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Miguel,

 

Please share your sample code in order to check it.

 

Regards

 

0 项奖励
回复

1,677 次查看
miguel_deprado
Contributor II

Here it is the benchmark: https://github.com/ekondis/mixbench

I have followed the openCL benchmark. The results come from the mixbench-ocl-ro binary.

The mixbench-ocl-alt binary runs on the imx8 quad-max but does not in the imx8m nano.

Thanks for your time

PD: I'd be interested to know whether you have any Vulkan benchmark to test on my machine.

标记 (1)
0 项奖励
回复

1,482 次查看
miguel_deprado
Contributor II

Hi,

no news?

 

Best regards