iMX8MQ evk with adv7535 no weston ui

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8MQ evk with adv7535 no weston ui

Jump to solution
1,599 Views
charleshuang
Senior Contributor II

Hi

Yocto zeus 5.4.70

I use imx8mq evk board and adv7535 bridge ic, but I can’t see the weston ui after booting up

I execute the following command then get weston service failed

root@imx8mqevk:~# systemctl -a | grep weston
* weston@root.service loaded failed failed Weston Wayland Compositor (on tty7)

Is this known issue?

Labels (1)
0 Kudos
1 Solution
1,556 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

You need change card from card0 to card1 in weston.ini

 

View solution in original post

0 Kudos
5 Replies
1,592 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Can you attach your boot and kernel log?

0 Kudos
1,575 Views
charleshuang
Senior Contributor II

The attached is log file

thanks

0 Kudos
1,570 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Which kind of images your are using? imx-image-multimedia? or imx-image-full

0 Kudos
1,568 Views
charleshuang
Senior Contributor II

We use imx-image-full

thanks

0 Kudos
1,557 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

You need change card from card0 to card1 in weston.ini

 

0 Kudos