iMX8MQ 8GB LPDDR4 part

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8MQ 8GB LPDDR4 part

1,967 Views
ani10c89
Contributor II

Hi,

As iMX8MQ supports upto 8GB LPDDR4 memory. Can you please suggest LPDDR4 8GB parts that are supported with iMX8M.

Regards,

Anirudha 

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

1,651 Views
Yuri
NXP Employee
NXP Employee

Hello,

  According to section 2.1.2 (Cortex-A53 Memory Map) of i.MX 8M Reference Manual, Rev. 0, 01/2018

only 4 GBytes address space is available for memory.

Regards,

Yuri.

0 Kudos
Reply

1,652 Views
ani10c89
Contributor II

Hi Yuri,

As per i.MX 8M Reference Manual section 9.1.1.1, it says up to 8GB memory capacity.

pastedImage_2.png

So we assumed 8GB should not be a issue. Can you please reconfirm if 8GB LPDDR4 is not supported.

Regards,

Anirudha

0 Kudos
Reply

1,652 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Section 9.1.1.1 concerns parameters of the DRAM controller as SNPS IP (taken separately by itself).

Restriction relates to address space, available for DRAM, in the i.MX8M SOC.  

Regards,

Yuri.

0 Kudos
Reply