iMX8MP Windows10 IoT Enterprise W21H2-1-4-1 About recovery from screen off

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8MP Windows10 IoT Enterprise W21H2-1-4-1 About recovery from screen off

280 Views
okuda
Contributor III

Hello.

Boot the OS using the W21H2-1-4-1 binary provided by NXP on the iMX8MP reference board.
After startup, the screen will turn off if left without any operation.
After confirming that the screen is off, operate the USB mouse to turn on the screen.

The time it takes for the screen to light up after operating the USB mouse is inconsistent.
(There are times when it is so slow that I feel that the OS is down.)

What is the cause of this?
Do you think it will be improved in future released versions?
I think this phenomenon will become a big problem if we try to release it as a product.

Thanks,
Koji Okuda.

 

0 Kudos
0 Replies