[iMX8MP-EVK] PCA6146 as interrupt controller?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[iMX8MP-EVK] PCA6146 as interrupt controller?

558 Views
khang_letruong
Senior Contributor III

Dear Community,

I would like to know if there's any conflict to configure the IO Expander PCA6146 on 8MPLUSEVK as interrupt-controller (i.e. one of the P0_x or P1_x as input to generate interruption on GPIO1_IO12) since  it is already used as gpio-controller, please?

Thanks in advance and best regards,

Khang

Labels (1)
0 Kudos
Reply
2 Replies

550 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @khang_letruong 

There is no conflict from the reference design

0 Kudos
Reply

548 Views
khang_letruong
Senior Contributor III

Hi @Zhiming_Liu ,

So do you confirm that it can be used as  gpio-controller to control some outputs and interrupt-controller to receive some inputs to trigger to interruption to the SoC at the same time?

BR,
K

0 Kudos
Reply