iMX8M mini and alexa (avs-device-sdk)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8M mini and alexa (avs-device-sdk)

1,269件の閲覧回数
flouveau
Contributor II

Hi community,

I integrate avs-device-sdk to a iMX8M mini dual core processor using Yocto (sumo).
This works pretty well.

I now try to play some music from amazon music unlimited, but I'm facing some issue at this point.
When I play radio from TuneIn, it works well.
When I play music from Amazon music, here is the log I get :

2020-02-10 13:52:26.719 [ 1f] 9 MediaPlayer:messageReceived:name=AudioMediaPlayer,type=error,source=aiurdemux0
2020-02-10 13:52:26.719 [ 1f] E MediaPlayer:handleBusMessageError:name=AudioMediaPlayer,source=aiurdemux0,error=GStreamer encountered a general stream error.,debug=../../../git/plugins/aiurdemux/aiurdemux.c(1078
)\: aiurdemux_push_task ()\: /GstPipeline\:audio-pipeline/GstDecodeBin\:decoder/GstAiurDemux\:aiurdemux0\:
streaming stopped\, reason error\, state 1
2020-02-10 13:52:26.719 [ 1f] 0 MediaPlayer:callingOnPlaybackError:name=AudioMediaPlayer,type=MEDIA_ERROR_INTERNAL_DEVICE_ERROR,error=GStreamer encountered a general stream error.,currentId=2
2020-02-10 13:52:26.719 [ 1f] 0 AudioPlayer:onPlaybackError:type=MEDIA_ERROR_INTERNAL_DEVICE_ERROR,error=GStreamer encountered a general stream error.,id=2
2020-02-10 13:52:26.719 [ 1f] 9 MediaPlayer:tearDownTransientPipelineElements:name=AudioMediaPlayer

No audio output.

I don't have any idea to find where this comes from.

Thanks for any help.
Regards,

Fabrice

ラベル(2)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,175件の閲覧回数
flouveau
Contributor II

I found a solution from the meta-avs-demo layer

mv /usr/lib/gstreamer-1.0/libgstaiurdemux.so /usr/lib/gstreamer-1.0/libgstaiurdemux.so.disabled

And start SampleApp.

=> Everything works fine. It seems that using full SW demuxing works better than using AIUR

0 件の賞賛
返信

1,175件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Good!

0 件の賞賛
返信