iMX8M mini + PCA9450A + SN65DSI83

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M mini + PCA9450A + SN65DSI83

1,269 Views
giacomobiancala
Contributor I

Hi,

On a custom board based on iMX8M mini, I am using PMIC PCA9450A and SN65DSI83 for MIPI-DSI to LVDS conversion.

Is it possible to use the same I2C1 (NVCC_I2C = 1,8V) for these 2 devices?

Do you think it could be a problem to add PCA9450 and SN65DSI83 to kernel?

Thanks,

Giacomo 

Labels (1)
0 Kudos
Reply
3 Replies

1,104 Views
igorpadykov
NXP Employee
NXP Employee

Hi Giacomo 

>Is it possible to use the same I2C1 (NVCC_I2C = 1,8V) for these 2 devices?

seems it is possible, as example of usage several devices on one i2c port one can look at

attached  i.MX6Q Sabre AI board schematic p.3 and linux documentation supporting that board on

i.MX Software and Development Tools | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,104 Views
giacomobiancala
Contributor I

Thank you,

Do you know if it is available a patch to add PCA9450A to kernel? This device is quite new.

Giacomo

0 Kudos
Reply

1,104 Views
igorpadykov
NXP Employee
NXP Employee

Hi Giacomo 

 

unfortunately I am not aware of such patch.

Best regards
igor

0 Kudos
Reply