iMX8M mini + PCA9450A + SN65DSI83

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8M mini + PCA9450A + SN65DSI83

1,187件の閲覧回数
giacomobiancala
Contributor I

Hi,

On a custom board based on iMX8M mini, I am using PMIC PCA9450A and SN65DSI83 for MIPI-DSI to LVDS conversion.

Is it possible to use the same I2C1 (NVCC_I2C = 1,8V) for these 2 devices?

Do you think it could be a problem to add PCA9450 and SN65DSI83 to kernel?

Thanks,

Giacomo 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,022件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Giacomo 

>Is it possible to use the same I2C1 (NVCC_I2C = 1,8V) for these 2 devices?

seems it is possible, as example of usage several devices on one i2c port one can look at

attached  i.MX6Q Sabre AI board schematic p.3 and linux documentation supporting that board on

i.MX Software and Development Tools | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,022件の閲覧回数
giacomobiancala
Contributor I

Thank you,

Do you know if it is available a patch to add PCA9450A to kernel? This device is quite new.

Giacomo

0 件の賞賛
返信

1,022件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Giacomo 

 

unfortunately I am not aware of such patch.

Best regards
igor

0 件の賞賛
返信