Hi,
I am trying to add two lane monochrome camera support to iMX8M Plus platform.
I tried to add changes to imx8-isi-cap.c and imx8-mipi-csi-sam.c files but i am not getting single frame.
The kernel version i am using is 5.4.
Could you please help me by providing patches for monochrome camera?
HI Dharanitharan:
Have you solved the issue ? I'm also porting a monochrome camera to imx8mp kernel5.4, but fail to get frame too.
Hi,
In our case, we changed the mipi clock source from continuous to gated. After that mipi-csi receiver in iMX8MP can able to receive frames.
HI Dharanitharan:
Got it ,thanks.
We have two MIPI camera interfaces on our boards using with our MIPI camera modules.
Our kernel is 5.10.9.
http://www.myirtech.com/list.asp?id=670
You can contact to get some information if needed.
Hi @joanxie
we are using 8 bit and 10 bit Gray format. The modifications are given in the attachment.
what detailed format do you use, and pls share your modification here
Hi @joanxie
Does iMX8M Plus support continuous mipi clock from sensor?
If yes, could you please provide us the kernel or device tree changes for continuous mipi clock support?
current bsp support continuous clock as default, you can refer to that
Hi @joanxie
Can you please help us by provide the kernel or device tree change or register setting to change mipi clock mode either from continuous to non-continuous mode or from non-continuous to continuous mode?
I am trying integrating monochrome sensor with iMX8M plus. With that i can receive frames only on non-continuous mode.
In continuous we are not receiving single frame in platform side. But we can see stream while probing the camera.
And below are some of the details provided in data sheet.
NOTE: Notice : Almost MIPI CSI2 block uses “ByteClk” from D- PHY. This “ByteClk” is not continuous
clock. User has to assert software reset when Camera module is turned off.
but I don't think current bsp supports non-continuous mode, do you mean you can set non-continuous mode on current bsp?