Hi NXP Community,
256MB of CMA memory has been successfully allocated in our iMX8M Plus based system with 1GB of DDR4:
root@viperimx8mp:~# dmesg | grep -i cma
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000070000000, size 256 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] Memory: 703092K/1015808K available (17920K kernel code, 1506K rwdata, 6920K rodata, 2880K init, 553K bss, 50572K reserved, 262144K cma-reserved)
However, I am struggling with following errors while streaming the camera with gstreamer :
root@viperimx8mp:~# gst-launch-1.0 v4l2src device=/dev/video2 ! video/x-raw, width=1920, height=1080, framerate=15/1 ! autovideos
On the debug console side :
root@viperimx8mp:~# [ 425.307460] enter isp_mi_stop
[ 425.942933] enter isp_mi_stop
[ 426.134422] cma: cma_alloc: alloc failed, req-size: 1013 pages, ret: -12
[ 426.143351] cma: cma_alloc: alloc failed, req-size: 1013 pages, ret: -12
[ 426.152091] cma: cma_alloc: alloc failed, req-size: 1013 pages, ret: -12
[ 426.160775] cma: cma_alloc: alloc failed, req-size: 1013 pages, ret: -12
[ 426.171442] cma: cma_alloc: alloc failed, req-size: 64 pages, ret: -12
[ 426.178547] cma: cma_alloc: alloc failed, req-size: 1013 pages, ret: -12
[ 426.189008] cma: cma_alloc: alloc failed, req-size: 1013 pages, ret: -12
[ 426.199560] cma: cma_alloc: alloc failed, req-size: 1013 pages, ret: -12
[ 426.209896] cma: cma_alloc: alloc failed, req-size: 1013 pages, ret: -12
[ 426.251559] enter isp_mi_stop
[ 426.381644] jxf355_set_fps : current frame length: 2252, current line length: 1280
[ 426.399852] enter isp_s_comp
[ 426.402763] enter isp_s_comp
[ 426.405644] enter isp_s_comp
[ 426.427504] enter wdr3_hw_init
[ 426.430580] wdr3 res: 1920 1080
[ 426.434753] enter isp_mi_start
Could you help if 256MB is sufficient for streaming single 1080p camera or the problem is somewhere else ?
Best Regards,
Khang
已解决! 转到解答。
Hi Khang,
I was facing same topic with my SoM. I found this link usefull
I assume it is controlled in the DTS in your case and you have to slightly increase your memsize.
resmem: reserved-memory {
/* global autoconfigured region for contiguous allocations */
linux,cma {
compatible = "shared-dma-pool";
reusable;
size = <0 0x38000000>;
alloc-ranges = <0 0x40000000 0 0x80000000>;
linux,cma-default;
};
Best regards
Holger
Hi Khang,
Can you please explain how you increased CMA size to 512MiB?
I have currently 640MiB allocated and I want to increase it as can be seen here:
~# dmesg | grep -i cma
[ 0.000000] Reserved memory: created CMA memory pool at 0x000000006a000000, size 640 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] Memory: 1034564K/2064384K available (18560K kernel code, 1644K rwdata, 7292K rodata, 3072K init, 552K bss, 374460K reserved, 655360K cma-reserved)
However the CMA size in the device tree does not correspond to 640MiB:
linux-imx/arch/arm64/boot/dts/freescale/imx8mp.dtsi
/* global autoconfigured region for contiguous allocations */
linux,cma {
compatible = "shared-dma-pool";
reusable;
size = <0 0x3c000000>;
alloc-ranges = <0 0x40000000 0 0xC0000000>;
linux,cma-default;
};
What is the correct way to increase this?
Thx
Hi @malik_cisse ,
Below is how I define 512MiB of CMA over 1024MiB (1 GiB) of DDR memory :
+ /* global autoconfigured region for contiguous allocations */
+ linux,cma {
+ compatible = "shared-dma-pool";
+ reusable;
+ size = <0 0x20000000>;
+ alloc-ranges = <0 0x40000000 0 0x40000000>;
+ linux,cma-default;
+ };
+ };
Small conversion : 0x20000000 = 536870912 B = 536870912/1024/1024=512 MiB.
In your initial case, it seemed that the size ranged from 0 to 960MiB = 1006632960/1024/1024 = 1006632960 B = 0x3c000000. But it resulted in 640MiB (less than expected 960MiB) because the alloc-range was not enough or not contiguous (the first allocable region has 1024MiB in size).
Regards,
K.
Hi @khang_letruong ,
Thank you for your insight. This clarifies things to a certain extend.
My SOM has 2GB of DDR memory and it should be possible to alloc 960MiB to CMA (that would be less than 50% of available DDR memory).
Would it make sense to set the alloc-range to the full 2GB DDR size (similarly to what you set in your DT) like this:
alloc-ranges = <0 0x80000000 0 0x80000000>; ??
PS:
I have the feeling the initial alloc-range in my device tree does not even reflect my actual DDR size
alloc-ranges = <0 0x40000000 0 0xC0000000>;
to me means that two DDR regions can be used for CMA
region1: 0 to 0x40000000 : 0x40000000 = 1073741824 Dec = 1073741824/1024/1024=1024MiB.
region2: 0 to 0xC0000000 :0xC0000000 = 3221225472 Dec = 3221225472/1024/1024=3072MiB.
1024MiB + 3072MiB = 4096MiB
Thus total DDR memory is 4GB and not expected 2GB. This can be an error from my SOM provider.
Hi @malik_cisse ,
I also have 2GB of DDR :
+ /* global autoconfigured region for contiguous allocations */
+ linux,cma {
+ compatible = "shared-dma-pool";
+ reusable;
+ size = <0 0x3c000000>;
+ alloc-ranges = <0 0x40000000 0 0x80000000>;
+ linux,cma-default;
+ };
and CMA is successfully allocated :
[ 0.000000] Reserved memory: created CMA memory pool at 0x000000005c000000, size 960 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] Memory: 714344K/2064384K available (19584K kernel code, 1608K rwdata, 6708K rodata, 3328K init, 644K bss, 367000K reserved, 983040K cma-reserved)
Brgs,
Khang
Hi @khang_letruong
This is just to confirm that CMA size is overwritten with other DTS. I can now change CMA also.
On the other side I found the root cause of my CMA memory leak:
Not freeing properly gstreamer appsink upon new pipeline stop/start cycle.
Thank you for sharing your thoughts.
You must be right. I just found a mistake on my side.
I just found a dtsi file that overrules and includes settings in imx8mp.dtsi and that sets the 640MiB.
&{/reserved-memory/linux,cma} {
size = <0 0x28000000>;
alloc-ranges = <0 0x40000000 0 0x60000000>;
};
I will now update the CMA setting here and give it a try.
Thank you again for the precious feedback.
Hi Khang,
I was facing same topic with my SoM. I found this link usefull
I assume it is controlled in the DTS in your case and you have to slightly increase your memsize.
resmem: reserved-memory {
/* global autoconfigured region for contiguous allocations */
linux,cma {
compatible = "shared-dma-pool";
reusable;
size = <0 0x38000000>;
alloc-ranges = <0 0x40000000 0 0x80000000>;
linux,cma-default;
};
Best regards
Holger
Hi @Holger75 ,
Thanks for sharing your experience. I temporarily solved the issue by setting the CMA size to 512MiB, which is a half of the available DDR memory in the system. I am not sure if the remain 512MiB would be sufficient for other running stuffs.
Best Regards,
Khang