iMX8 uSDHC SD3.0 tuning

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX8 uSDHC SD3.0 tuning

1,013 次查看
mileswang
Contributor II

Dear sir,

I'm confused about the SD3.0 tuning.

In iMX8RM, there is a register "uSDHCx_TUNING_CTRL", bit 24 - STD_TUNING_EN. If the bit is set, standard tuning circuit and procedure enable. I want to know what is "standard tuning", how to do standard tuning. There should be "non-standard tuning", how to do "non-standard tuning"?

In  register "uSDHCx_MIX_CTRL", bit 24 - AUTO_TUNE_EN; bit 22 - EXE_TUNE. How to do auto-tune? and how to do manual-tune? Do auto-tune have relation with "standard tuning" or "non-standard tuning".

By my understanding, there should be 4 possibility:

1. standard tuning by auto-tune;

2. standard tuning by manual-tune;

3. non-standard tuning by auto-tune;

4. non-standard tuning by manual-tune.

Is it correct? I really don't know how to do tuning. I need a note to describe how to do it.

Thanks,

Miles

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

774 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Look at the following discussion, where some details of different tuning procedure are 

shown: 

https://community.nxp.com/message/1025457?commentID=1025457#comment-1025457 

iMX7D SDIO tuning debugging 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 项奖励
回复