iMX6ul evk board sai1 using

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6ul evk board sai1 using

506 Views
ATAineri
Contributor III

There is no SAI on iMX6ul EVK board. I found that CSI on board can be multiplexing like SAI1 for iMX6ul. Moreover there is i2c that I need for my external audio device.

Can I solder my connector to this pins I need? Or maybe the binding of these pins does not meet the standards of i2s and this lines is totally incompatible for I2S using?

IMG_20191108_221020.jpgScreenshot from 2019-11-08 22-21-34.png

Labels (2)
0 Kudos
Reply
1 Reply

464 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

>>Can I solder my connector to this pins I need?

Yes, you can.

But in device tree, you should ask software engineer to remove configurations on Camera. and add IOMUX of CSI pins( Multiplexed them to be SAI1 pins)

>>Or maybe the binding of these pins does not meet the standards of i2s and this lines is totally incompatible for I2S using?

These pins supports the standards of i2s, usage is fully same as that of SAI2 with I2S connection, see EVK schematic, please!

Have a nice day!

BR,

Weidong

0 Kudos
Reply