Now my pcie rc mode is working fine, it can enumerate an ep device(pcie to uart xr17v35x) properly.The software is imx6_platform_sdk_v1.1.0 (NO OS)
promblem:
(1)I would like to use Two i. mx6q boards, one is used as PCIe RC. The other one is used as PCIe EP,As shown in the photo below
My test routine is based on imx6_platform_sdk_v1.1.0, only pcie_test_rc.c, and I need an ep routine. Can you help me provide a pcie_test_ep.c routine, preferably based on imx6_platform_sdk_v1.1.0 (NO OS), or other routines and materials, I will be very grateful to you! My email address is 371554161@qq.com.
Best Regards
yong luo.
Hi yong
I am not aware of baremeta or platform_sdkl pcie ep examples, however
one can look at patches provided on
i.MX6Q PCIe EP/RC Validation System
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------