Hi m.c.
datasheet is correct, usb connections are described in sect.3.9.14.1 Pad/Package/Board connections:
The USBx_VBUS pin cannot directly connect to the 5 V VBUS voltage on the USB2.0 link.
Each USBx_VBUS pin must be isolated by an external 30 K 1% precision resistor.
i.MX 8M Mini Applications Processor Datasheet for Consumer Products
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------