iMX6UL U-Boot 2019.04 doesn't boot from flash if not signed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6UL U-Boot 2019.04 doesn't boot from flash if not signed

Jump to solution
836 Views
MikeEngel
Contributor IV

We have ported our module to the new 2019.04 U-boot and have seen that our u-boot will not boot from NAND when SECURE_BOOT is enabled. But it will boot from RAM using uuu tool.

 

Why is it now necessary to sign the U-boot with this new version?

In the previous version we used 2017.03 that was not necessary using the same configuration

 

Is the HAB events checked during boot and if that fails u-boot will not start?

 

Best regards,

--

Mike Engel

0 Kudos
Reply
1 Solution
763 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  Please let me know more details about the issue.

1.

   The following U-boot release is used, correct?

uboot-imx - i.MX U-Boot 

 2.

 U-boot configuration:  CONFIG_SECURE_BOOT=y

 i.MX 6UL fuse SEC_CONFIG[1] =0 (open)

 

3.

  Uboot does not boot from NAND and it boots if  CONFIG_SECURE_BOOT=n

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

View solution in original post

0 Kudos
Reply
1 Reply
764 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  Please let me know more details about the issue.

1.

   The following U-boot release is used, correct?

uboot-imx - i.MX U-Boot 

 2.

 U-boot configuration:  CONFIG_SECURE_BOOT=y

 i.MX 6UL fuse SEC_CONFIG[1] =0 (open)

 

3.

  Uboot does not boot from NAND and it boots if  CONFIG_SECURE_BOOT=n

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply