iMX6SX ethernet MAC clock timing delay

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6SX ethernet MAC clock timing delay

857 Views
msarwar
Contributor III

Hi guys,

 

Hope you're all well. I am planning to connect an sja1105E ethernet switch to an iMX6SX. In the SJA1105E datasheet it says an external delay of 1.5 - 2.0 nS is required between the host rgmii interface and the switch port that the host uses (6.2.3 of NXP SJA1105E datasheet).

 

In the reference manual of the iMX6SX, section 24.5.5 Ethernet Control Register, there are a couple of bits, RXC_DLY and TXC_DLY, which select delayed versions of the clock:

msarwar_0-1654593009086.png

 

So, my question is, does setting those bits fulfil the requirements of the delayed clocks required by the RGMII interface ? If so is there any example configuration I can check ?

 

If the answer is no, does that mean an external board delay is required ?

 

thanks,

Mahtab

 

 

 

 

Labels (2)
0 Kudos
Reply
1 Reply

828 Views
msarwar
Contributor III

Hi all,

 

I would appreciate a response to this question, thank you.

 

regards,

msarwar

0 Kudos
Reply