iMX6Q Voltage of CSI parallel pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6Q Voltage of CSI parallel pins

600件の閲覧回数
herveschmitt
Contributor II

We didn't find information on the voltage constraints of PIXCLK, HSYNC, VSYNC, DATA[0..7] in the IMX6DQIEC.

We checked the signals using an OV5652 module (natively supported by the Freescale BSP) that have an amplitude of 3.3V.

We are now working on a camera module powered with 1.8V and wonder if it can work "as is" or require some level shifters 1.8V -> 3.3V.

TIA.

ラベル(1)
0 件の賞賛
返信
1 返信

492件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Herve

NVCC_CSI is voltage domain of PIXCLK, HSYNC, VSYNC, DATA[0..7] in the IMX6DQIEC,

so it is necessary to power it with 1.8V for operation with sensor with 1.8V levels

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信