iMX6Q Voltage of CSI parallel pins

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX6Q Voltage of CSI parallel pins

601 次查看
herveschmitt
Contributor II

We didn't find information on the voltage constraints of PIXCLK, HSYNC, VSYNC, DATA[0..7] in the IMX6DQIEC.

We checked the signals using an OV5652 module (natively supported by the Freescale BSP) that have an amplitude of 3.3V.

We are now working on a camera module powered with 1.8V and wonder if it can work "as is" or require some level shifters 1.8V -> 3.3V.

TIA.

标签 (1)
0 项奖励
回复
1 回复

493 次查看
igorpadykov
NXP Employee
NXP Employee

HI Herve

NVCC_CSI is voltage domain of PIXCLK, HSYNC, VSYNC, DATA[0..7] in the IMX6DQIEC,

so it is necessary to power it with 1.8V for operation with sensor with 1.8V levels

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复