Dear All,
We are using RS232 DTE mode full function of UART1 on iMX6Q.
Could anyone tell me how to enable DTE mode full function on UART1?
We now is set DTE mode via register "2020090" But system will hang on.
We tried to disconnect DCD pin, the hang on status will be solved,
I think isn't where setting is wrong?
Please give me suggestion.
Thank a lot.
已解决! 转到解答。
Sean
After Fushi's reply, do you still have further question? If not please, keep exchanging email with him, otherwise please click Corret Answer/Helpful Answer. We would like to close the discussion if no activity in 3 days.
Thanks,
Yixing
Hi ,
Please reference the board file of iMX6Q arm2.
static const struct imxuart_platform_data mx6_arm2_uart1_data __initconst = {
.flags = IMXUART_HAVE_RTSCTS | IMXUART_USE_DCEDTE | IMXUART_SDMA, /*this line enable DTE*/
.dma_req_rx = MX6Q_DMA_REQ_UART2_RX,
.dma_req_tx = MX6Q_DMA_REQ_UART2_TX,
};
But the arm2 board only use RTS CTS RXD TXD pins, seems you use DB9 connector , right ?
Please configure your IOMUX carefully , check iMX6 RM section 64.4.3 , such as :
64.4.3.6 DCD_B - Data Carrier Detect
This signal is an output in DCE mode and an input in DTE mode. If used, the DCE
device uses this signal to inform the DTE it has detected the carrier signal and the
connection will be set up. This signal remains active while the connection remains
established.
In DTE mode this input can trigger an interrupt on changing state. This is achieved by
setting to '1' the interrupt enable bit (DCD, UCR3[9]). The change state is reflected in
DCDDELT (USR2[6]). Also, the state of the Data Carrier Detect input is mirrored in the
status register DCDIN (USR2[5]).
Hi, Fushi and Sean,
This afternoon, I changed board-mx6q_sabresd.h and board-mx6q_sabresd.c in order to add other 6 pins (except for ground pin), then follow SabreAI settings by adding imxuart_platform_data and modifying mx6q_sabresd_init_uart. Then, system does not start up completely for login via telnet.
Remarked DCD, DTR, DSR, and RI from board-mx6q_sabresd.h, and leave all changes in board-mx6q_sabresd.c, then, I am able to telnet system and memtool -32 0x2020090 1 shows 0xb41 (which stands for DTE mode). Use telnet, because console does not response in DTE mode.
Added DTR, DSR and DCD into board-mx6q_sabresd.h, I am able to telnet into system and memtool -32 0x2020090 1 shows 0xb41. Post telnet log below:
$ telnet 192.168.106.101
Trying 192.168.106.101...
Connected to 192.168.106.101.
Escape character is '^]'.
Welcome to Freescale Semiconductor Embedded Linux Environment
freescale login: root
root@freescale ~$ /unit_tests/memtool -32 0x2020090 1
E
Reading 0x1 count starting at address 0x02020090
0x02020090: 00000B41
Please note, if enable RI on i.MX6Q SabreSD, I cannot telnet into system. Possible reason is that i.MX6Q SabreSD uses EB3 as boot mode selector and I did not rework hardware for this verification. On customer site, RI works fine, so I ignore RI error at this moment.
Append modified board-mx6q_sabresd.h and board-mx6q_sabresd.c for your reference.
Dear Wilson,
Our board with pull-high EIM_D23 works.
However, it's just for debug.
Our application utilizes this pin by connecting it to MAX3243CPW (RS-232 receiver) and it hangs the system.
Could you test this again with similar hardware layout or give some advice?
Thanks.
BRs,
ZL
We have written 1 to clear DTRD bit of UART1_USR1 in interrupt routine(imx_int(int irq, void *dev_id), drivers/tty/serial/imx.c ).
However, the interrupts still happen continuously. and now UART1_USR1=0x2040.
Dear Fushi Peng,
We tried to debug in driver source(kernel_imx/drivers/tty/serial/imx.c) and add some message in interrupt routines.
When device is DCE mode, the interrupts happen one or two times for each read/write command.
When device is DTE mode, the interrupts happen continuously, and UART1_USR1=0x20C0
Therefore, I think the hang-up is caused by abnormal interrupts in DTE mode.
How do we to fix this issue?
Please help!!!!!
Dear Fushi Peng,
Thanks for your help.
We tried to config UART1 IOMUX but system still hang on when config to DTE mode.
Could you have any suggestion for us?
The following code is our UART1 config.
static const struct imxuart_platform_data mx6_uart_pdata __initconst = {
.flags = IMXUART_HAVE_RTSCTS | IMXUART_USE_DCEDTE ,
};
imx6q_add_imx_uart(0, &mx6_uart_pdata);
Thank you so much.