How to control the USB_OTG_PWR and the USB_H1_PWR of i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to control the USB_OTG_PWR and the USB_H1_PWR of i.MX6

Jump to solution
2,132 Views
yuuki
Senior Contributor II

I understand that USB_OTG_PWR and USB_H1_PWR are the signals which control each VBUS of USB OTG and USB Host1.

These signals are assigned to the following pins.

- USB_OTG_PWR : EIM_D22(ALT4) or KEY_ROW4(ALT2)
- USB_H1_PWR : EIM_D31(ALT6) or GPIO_0(ALT6)
"To control PMIC to supply VBUS voltage"

However, I cannot find the register bit filde for controlling these signals.
Could you teach register bit filde which controls these signals?

Best Regards,

0 Kudos
1 Solution
1,301 Views
alfred_liu
NXP Employee
NXP Employee

Hi, YUuki

these two signals are just alike normal GPIO, no special register for USB_OTG_PWR and USB_H1_PWR.


View solution in original post

0 Kudos
2 Replies
1,301 Views
alfred_liu
NXP Employee
NXP Employee


Hi, Yuuki

consulted with BSP team.

they treated these two signals as normal GPIO in linux till now.

1,302 Views
alfred_liu
NXP Employee
NXP Employee

Hi, YUuki

these two signals are just alike normal GPIO, no special register for USB_OTG_PWR and USB_H1_PWR.


0 Kudos