iMX6Q/S CSI capture from FPGA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6Q/S CSI capture from FPGA

890件の閲覧回数
jaroslaw_glazow
Contributor I

Hello all,
I have a question a little bit on a silly side. I have a FPGA unit which outputs pre-configured 1080@30 fps video (with typical parameters one can see in such signals), and I want to capture it with gstreamer (v4l2). I managed to capture this video on other vendor SOCs while working on other projects, but I have no clue how to capture it with IMX, my naive approach was to strip-down existing drivers (ov5640 or tc358743), but my lack of knowledge about driver development on iMX slows me down. Is there any simpler way?

Best regards,
Jarek 

ラベル(2)
タグ(1)
0 件の賞賛
2 返答(返信)

765件の閲覧回数
zhouqi
Contributor II

Hi Jarek 

   sorry to interrupt you

    Have you solved this problem later?

    I get the same porblem now? Can you give me some suggestion or your solution way.

   Thank you very much .

Best regards

zhou

    

0 件の賞賛

791件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jarek 

one can look at Chapter 21 Configuring the Camera Preview Driver

sdk document included in "1.1.0_iMX6_Platform_SDK.zip" on

SMP Enable in IMX6 

Linux/Android tutorials:

Android Camera - Variscite Wiki 

Parallel camera | ConnectCore 6 

15. i.MX Video Capture Driver — The Linux Kernel documentation 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛