[iMX6Q] No SDCLK for DDR3.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[iMX6Q] No SDCLK for DDR3.

ソリューションへジャンプ
836件の閲覧回数
chilwonna
Contributor II

Hi,

I made a new board from SABRESDP_C5.

DDR3's configuration is  same with SABRESDP_C5.

But, I have a big problem about DDR3.

In DDR Stress Test Tool,

Address and Data lines is generated. But SDCLK is not.

I need a help. Please advise.

ラベル(1)
タグ(3)
0 件の賞賛
1 解決策
709件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi chillwona

probably these traces are shorted or broken, may be recommended

to check layout. Also please check Chapter 8 Avoiding Board Bring-up Problems

i.MX6 System Development User’s Guide (rev.1, 6/2013)

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
709件の閲覧回数
chilwonna
Contributor II

thanks.

solved.

0 件の賞賛
710件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi chillwona

probably these traces are shorted or broken, may be recommended

to check layout. Also please check Chapter 8 Avoiding Board Bring-up Problems

i.MX6 System Development User’s Guide (rev.1, 6/2013)

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛