Hello. I am using iMX6UL processor and I need to start watchdog timer by external signal. Is there such feature? Can watchdog timer starts by extrenal signal (GPIO, for example)?
In manual reference described external signals WDOG1_ANY and WDOGx_B as Input/Output signals, but I can't understand what is their purpose as input signals.
Hello,
There is no explicit input pin to trigger WDOG start in hardware way.
Customers can use a GPIO for interrupt, assuming that interrupt service
code starts the WDOG if it was not yet working.
Have a great day,
Yuri
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.