I am going through the document called Freescale Yocto Project User's Guide (IMXLXYOCTOUG, Rev. L3.14.38_6ul-ga, 09/2015)
I followed all the steps to setup the iMX/Yocto environment on Linux. I am running into an issue when I run the bitake command described in "5.3 Building an image".
The following error below is displayed in my console, what is missing?
xxxx@xxxx-VirtualBox:~/build_dir_imx6ulevk$ bitbake fsl-image-machine-test
ERROR: Traceback (most recent call last):
File "/home/xxxx/fsl-release-bsp/sources/poky/bitbake/lib/bb/cookerdata.py", line 175, in wrapped
return func(fn, *args)
File "/home/xxxx/fsl-release-bsp/sources/poky/bitbake/lib/bb/cookerdata.py", line 185, in parse_config_file
return bb.parse.handle(fn, data, include)
File "/home/xxxx/fsl-release-bsp/sources/poky/bitbake/lib/bb/parse/__init__.py", line 107, in handle
return h['handle'](fn, data, include)
File "/home/xxxx/fsl-release-bsp/sources/poky/bitbake/lib/bb/parse/parse_py/ConfHandler.py", line 118, in handle
abs_fn = resolve_file(fn, data)
File "/home/xxxx/fsl-release-bsp/sources/poky/bitbake/lib/bb/parse/__init__.py", line 130, in resolve_file
raise IOError("file %s not found" % fn)
IOError: file /home/xxxx/sources/poky/meta/conf/layer.conf not found
ERROR: Unable to parse /home/xxxx/sources/poky/meta/conf/layer.conf: file /home/xxxx/sources/poky/meta/conf/layer.conf not found
xxxx@xxxx-VirtualBox:~/build_dir_imx6ulevk$
Extra information: my platform is i.MX6 ULEVK
Can you share complete path of fsl-release-bsp . I am having a similar issue with i.MX8