iMX6 SoloX MQX Kernel & Uboot Patches From AN5127

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX6 SoloX MQX Kernel & Uboot Patches From AN5127

跳至解决方案
1,116 次查看
jeremym
Contributor IV

I cannot locate the two patches mentioned in AN5127:

0001-Kernel-M4-Reserve-16M-DDR-memory-for-M4-core-use.patch

0001-U-Boot-M4-Reserve-16M-DDR-memory-for-M4-core-use.patch

Does anyone know where to locate these?

thanks,

jeremy

标签 (1)
标记 (3)
1 解答
742 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Jeremy McClintock,

These patches are no longer available on the git mentioned on the AN, but please find them attached.

Regards,

在原帖中查看解决方案

5 回复数
742 次查看
jeremym
Contributor IV

Hi Victor - any update on the location of the patches?  Thanks, Jeremy

0 项奖励
743 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Jeremy McClintock,

These patches are no longer available on the git mentioned on the AN, but please find them attached.

Regards,

742 次查看
jeremym
Contributor IV

Thank you very much, it's appreciated.

742 次查看
b36401
NXP Employee
NXP Employee

You can get them with git as mentioned in the Application Note.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
742 次查看
jeremym
Contributor IV

Hi Victor - the application note doesn't describe where to fetch the patch from.  It simply states to navigate to a particular folder and then attempt to apply the patch.  The patch was not part of the distribution when I fetched/cloned.  If I attempt to follow the application note as described, I get:

/usr/lib/git-core/git-am: 209: /usr/lib/git-core/git-am: cannot open 0001-Kernel-M4-Reserve-16M-DDR-memory-for-M4-core-use.patch: No such file