Dear experts--
I need to connect an LCD with a System-80 (Aka. Intel-80) to an iMX6 Solo (8-bit Async Parallel i/f)
According to the Reference Manual, the IPUv3 DI has support for this interface, but I read an old thread that the Linux BSP drivers do not include support.
Has this support be added in more recent releases?
Has anyone successfully connected a System-80 LCD to an IMX6?
Sincerely,
Erez
已解决! 转到解答。
Attached is the system 80 LCD patch for iMX51 3DS board, maybe you can reference to it.
The panel is GPM722A0, the controller chip is ILI9320.
I don't know of anyone here that has done that, but Qiang Li is right, there is no driver available, you would need to develop it.
Best regards,
Sergio
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------