iMX6 + KSZ9031: uboot dhcp after sw reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 + KSZ9031: uboot dhcp after sw reset

1,260 Views
joanvicient
Contributor II

Hi there, we are using a board with an iMX6QP and a KSZ9031.

When we power the board we have 1GBps connection without a problem in both uboot and kernel.

The problem is that after a reboot, we cannot get ip address from dhcp in uboot.

If we boot from Nand, kernel can fix the mac/phy/dhcp issue.

Any ideas about what is happening? Thanks in advance for your help!

The u-boot log error is:

U-Boot 2017.03+g3cd63a0cef (Sep 06 2019 - 09:40:31 +0000)

CPU: Freescale i.MX6QP rev1.0 at 792MHz
CPU: Industrial temperature grade (-40C to 105C) at 39C
Reset cause: WDOG
DRAM: 1 GiB
NAND: 128 MiB
MMC: FSL_SDHC: 0
In: serial
Out: serial
Err: serial
Net: FEC [PRIME]
Autoboot in 2 seconds
=> dhcp
BOOTP broadcast 1
BOOTP broadcast 2
BOOTP broadcast 3
BOOTP broadcast 4
BOOTP broadcast 5
BOOTP broadcast 6
BOOTP broadcast 7
BOOTP broadcast 8
BOOTP broadcast 9

The uboot code is:

/* rgmi enet */
static iomux_v3_cfg_t const enet_pads[] = {
MX6_PAD_ENET_MDIO__ENET_MDIO | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_MDC__ENET_MDC | MUX_PAD_CTRL(ENET_PAD_CTRL),

MX6_PAD_RGMII_TXC__RGMII_TXC | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_RGMII_TX_CTL__RGMII_TX_CTL | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_RGMII_TD0__RGMII_TD0 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_RGMII_TD1__RGMII_TD1 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_RGMII_TD2__RGMII_TD2 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_RGMII_TD3__RGMII_TD3 | MUX_PAD_CTRL(ENET_PAD_CTRL),

MX6_PAD_RGMII_RXC__RGMII_RXC | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_RGMII_RX_CTL__RGMII_RX_CTL | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_RGMII_RD0__RGMII_RD0 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_RGMII_RD1__RGMII_RD1 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_RGMII_RD2__RGMII_RD2 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_RGMII_RD3__RGMII_RD3 | MUX_PAD_CTRL(ENET_PAD_CTRL),

MX6_PAD_ENET_REF_CLK__ENET_TX_CLK | MUX_PAD_CTRL(ENET_PAD_CTRL),

MX6_PAD_ENET_CRS_DV__GPIO1_IO25 | MUX_PAD_CTRL(ENET_PAD_CTRL), /*int*/
MX6_PAD_ENET_TX_EN__GPIO1_IO28 | MUX_PAD_CTRL(ENET_PAD_CTRL), /*rst*/
};

static int reset_enet_phy()
{
/* Reset KSZ9031 PHY */
gpio_request(GPIO_ETH_RESET, "GPIO_ETH_RESET");

gpio_direction_output(GPIO_ETH_RESET, 0);
mdelay(10);
gpio_set_value(GPIO_ETH_RESET, 1);
mdelay(100);

gpio_free(GPIO_ETH_RESET);
return 0;
}

int board_phy_config(struct phy_device *phydev)
{
/* Joan: errata 5: Autonegotiation link-up failure due FLP interval */
ksz9031_phy_extended_write(phydev, 0x0, 0x3, MII_KSZ9031_MOD_DATA_NO_POST_INC, 0x1A80);
ksz9031_phy_extended_write(phydev, 0x0, 0x4, MII_KSZ9031_MOD_DATA_NO_POST_INC, 0x0006);

///tret de udoo, apalis no ho te: ho deixo per defecte
phy_write(phydev, MDIO_DEVAD_NONE, MII_CTRL1000, 0x1c00);

/* control data pad skew - devaddr = 0x02, register = 0x04 */
ksz9031_phy_extended_write(phydev, 0x02,
MII_KSZ9031_EXT_RGMII_CTRL_SIG_SKEW,
MII_KSZ9031_MOD_DATA_NO_POST_INC, 0);
/* rx data pad skew - devaddr = 0x02, register = 0x05 */
ksz9031_phy_extended_write(phydev, 0x02,
MII_KSZ9031_EXT_RGMII_RX_DATA_SKEW,
MII_KSZ9031_MOD_DATA_NO_POST_INC, 0);
/* tx data pad skew - devaddr = 0x02, register = 0x06 */
/*ksz9031_phy_extended_write(phydev, 0x02,
MII_KSZ9031_EXT_RGMII_TX_DATA_SKEW,
MII_KSZ9031_MOD_DATA_NO_POST_INC, 0);*/
/* gtx and rx clock pad skew - devaddr = 0x02, register = 0x08 */
ksz9031_phy_extended_write(phydev, 0x02,
MII_KSZ9031_EXT_RGMII_CLOCK_SKEW,
MII_KSZ9031_MOD_DATA_NO_POST_INC, 0x03FF);

if (phydev->drv->config)
phydev->drv->config(phydev);

return 0;
}

int board_eth_init(bd_t *bis)
{

imx_iomux_v3_setup_multiple_pads(enet_pads, ARRAY_SIZE(enet_pads));
reset_enet_phy();
return cpu_eth_init(bis);
}

img1.pngimg2.png

Labels (3)
0 Kudos
1 Reply

954 Views
igorpadykov
NXP Employee
NXP Employee

Hi joan

one can check if KSZ9031 was correctly reset and its power-up sequence

according to its datasheet. In general such issues may happen when reboot

performing without full board reset as it is done in NXP i.MX6QP Sabre SD

reference board (p.21 U507, with WDOG_B and PWRON SPF-28857.pdf schematic)

Design files, including hardware schematics, Gerbers, and OrCAD files for i.MX 6QuadPlus (i.MX 6Dual...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos