iMX solo Ethernet MDC and MDIO voltage level

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX solo Ethernet MDC and MDIO voltage level

645件の閲覧回数
aabhishekoct18
Contributor III

Hi Team 

I have connected NVCC_ENET =3.3V and  NVCC_RGMM=2.5V can you please  let me know . what should be VIH and VOH level of  these  pin. 

ラベル(1)
0 件の賞賛
返信
1 返信

598件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Abhishek 

according to Table 97. 21 x 21 mm Functional Contact Assignments they belong to

NVCC_ENET power domain. Levels are defined by Table 23. GPIO DC Parameters

i.MX 6Solo/6DualLite Applications Processors for Consumer Products

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信