Hello,
Hope the following helps.
https://community.nxp.com/message/926823
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer
button. Thank you!
hello ,Mr. Yuri Muhin, I have successfully configured the pin, but what happens is that the pin is always output low level after power off to power on about reset.
Hello,
You can test WDOG functionality, using software reset bit WDA of Watchdog Control Register (WDOG_WCR).
WDOG_B signal remains asserted as long as the WDA bit is "0".
Note, because of total system reset, performed by the board circuit, WDA will be also reset in default state ("1")
just after the WDOG reset.
Regards,
Yuri.
thanks