i.mx8qm MEK FLEXCAN issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx8qm MEK FLEXCAN issue

1,363 次查看
aksh9354
Contributor I

hello,

I am using the i.mx8qm MEK board,

facing the issue while the board sends the first message on can bus, the bus is going in off state but if another node or host pc sends the first message on the can bus there is no any issue the communication is fine 

 

 bus-off issue

imx_to_hostpc.png

0 项奖励
9 回复数

1,299 次查看
aksh9354
Contributor I

I tried it but still it not opening showing below error

An invalid set of parameters has been specified in the url.

0 项奖励

1,313 次查看
aksh9354
Contributor I

the article is not available on this link

0 项奖励

1,306 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

You can not open it https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Simple-CAN-FD-test-on-i-MX8QXP-s-MEK-boa... you can to try it again, and log in community first. It works well on my side, if it still not work contact me.

0 项奖励

1,320 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport
0 项奖励

1,321 次查看
aksh9354
Contributor I

yes i am using the base board

 

0 项奖励

1,336 次查看
aksh9354
Contributor I

i am using i.mx8qm mek board for adas project.....

0 项奖励

1,323 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Have you using the base board with the i.mx8qm MEK board?https://www.nxp.com/part/MCIMX8-8X-BB#/

As there are 2 can support on the base board.

0 项奖励

1,340 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using the base board?

0 项奖励

1,362 次查看
aksh9354
Contributor I

error showing

root@imx8qmmek:~# ip -details link show can0
2: can0: <NOARP,UP,LOWER_UP,ECHO> mtu 16 qdisc pfifo_fast state UNKNOWN mode DEFAULT group default qlen 10
    link/can  promiscuity 0
    can state ERROR-ACTIVE (berr-counter tx 0 rx 0) restart-ms 0
          bitrate 500000 sample-point 0.875
          tq 50 prop-seg 17 phase-seg1 17 phase-seg2 5 sjw 1
          flexcan: tseg1 2..64 tseg2 1..32 sjw 1..32 brp 1..1024 brp-inc 1
          flexcan: dtseg1 1..39 dtseg2 1..8 dsjw 1..8 dbrp 1..1024 dbrp-inc 1
          clock 40000000numtxqueues 1 numrxqueues 1 gso_max_size 65536 gso_max_segs 65535

0 项奖励